TI BLE5-Stack API Documentation  9.14.00
Data Fields
CS_modeThreeStep_t Struct Reference

Data Fields

uint8_t antennaPermutationIndex
 Antenna permutation index. More...
 
modeTwoStepData_t data []
 Array of length (numAntennaPath + 1), each element is of type modeTwoStepData_t. More...
 
uint8_t packetAntenna
 PacKet antenna. More...
 
uint8_t packetNadm
 Attack likelihood. More...
 
uint8_t packetQuality
 Packet quality. More...
 
uint8_t packetRssi
 Packet RSSI. More...
 
uint16_t ToDToA
 Time difference in 0.5 ns units between arrival and departure of CS packets. More...
 

Field Documentation

§ antennaPermutationIndex

uint8_t antennaPermutationIndex

Antenna permutation index.

§ data

Array of length (numAntennaPath + 1), each element is of type modeTwoStepData_t.

§ packetAntenna

uint8_t packetAntenna

PacKet antenna.

§ packetNadm

uint8_t packetNadm

Attack likelihood.

§ packetQuality

uint8_t packetQuality

Packet quality.

§ packetRssi

uint8_t packetRssi

Packet RSSI.

§ ToDToA

uint16_t ToDToA

Time difference in 0.5 ns units between arrival and departure of CS packets.


The documentation for this struct was generated from the following file:
© Copyright 1995-2025, Texas Instruments Incorporated. All rights reserved.
Trademarks | Privacy policy | Terms of use | Terms of sale