![]() |
![]() |
|
TI BLE5-Stack API Documentation
9.14.00
|
Data Fields | |
| uint8_t | addr [B_ADDR_LEN] |
| Address of the advertising device. More... | |
| uint8_t | addrType |
| Public, random, public ID, random ID, or anonymous. More... | |
| uint8_t | advSid |
| SID (0x00-0x0f) of the advertising PDU. 0xFF means no ADI field in the PDU. More... | |
| uint16_t | dataLen |
| Length of the data. More... | |
| uint8_t | directAddr [B_ADDR_LEN] |
| TargetA address. More... | |
| uint8_t | directAddrType |
| Type of TargetA address in the directed advertising PDU. More... | |
| uint8_t | evtType |
| uint8_t * | pData |
| Pointer to advertising or scan response data. More... | |
| uint16_t | periodicAdvInt |
| Periodic advertising interval. 0 means no periodic advertising. More... | |
| uint8_t | primPhy |
| PHY of the primary advertising channel. More... | |
| int8_t | rssi |
| -127 dBm <= RSSI <= 20 dBm More... | |
| uint8_t | secPhy |
| PHY of the secondary advertising channel. More... | |
| int8_t | txPower |
| -127 dBm <= TX power <= 126 dBm More... | |
| uint8_t addr[B_ADDR_LEN] |
Address of the advertising device.
| uint8_t addrType |
Public, random, public ID, random ID, or anonymous.
| uint8_t advSid |
SID (0x00-0x0f) of the advertising PDU. 0xFF means no ADI field in the PDU.
| uint16_t dataLen |
Length of the data.
| uint8_t directAddr[B_ADDR_LEN] |
TargetA address.
| uint8_t directAddrType |
Type of TargetA address in the directed advertising PDU.
| uint8_t evtType |
Bits 0 to 4 indicate connectable, scannable, directed, scan response, and legacy respectively
| uint8_t* pData |
Pointer to advertising or scan response data.
| uint16_t periodicAdvInt |
Periodic advertising interval. 0 means no periodic advertising.
| uint8_t primPhy |
PHY of the primary advertising channel.
| int8_t rssi |
-127 dBm <= RSSI <= 20 dBm
| uint8_t secPhy |
PHY of the secondary advertising channel.
| int8_t txPower |
-127 dBm <= TX power <= 126 dBm