TI BLE5-Stack API Documentation
9.14.00
.build.ble5.cc23xx
api-sources
ble-core
source
ti
ble
stack_util
icall
app
icall_addrs.h
Go to the documentation of this file.
1
/******************************************************************************
2
3
Group: WCS, BTS
4
$Target Device: DEVICES $
5
6
******************************************************************************
7
$License: BSD3 2013 $
8
******************************************************************************
9
$Release Name: PACKAGE NAME $
10
$Release Date: PACKAGE RELEASE DATE $
11
*****************************************************************************/
12
18
#ifndef ICALLADDRS_H
19
#define ICALLADDRS_H
20
21
#include "
ti/ble/stack_util/icall/app/icall.h
"
22
23
#ifndef USE_DEFAULT_USER_CFG
24
25
#include "
ti/ble/stack_util/comdef.h
"
26
#include "ti/ble/app_util/config/ble_user_config.h"
27
28
extern
icall_userCfg_t
user0Cfg
;
29
35
#define USER0_CFG &user0Cfg
36
37
#else
38
39
#define USER0_CFG NULL
40
41
#endif // USE_DEFAULT_USER_CFG
42
// end of ICall_Constants
44
50
extern
void
startup_entry
(
const
ICall_RemoteTaskArg
*arg0,
void
*arg1 );
51
//extern ICall_RemoteTaskEntry startup_entry;
52
#define ICALL_ADDR_MAPS \
53
{ \
54
(ICall_RemoteTaskEntry) (startup_entry) \
55
}
56
68
#define ICALL_TASK_STACK_SIZES { 1500 }
69
76
#define ICALL_CUSTOM_INIT_PARAMS { USER0_CFG }
77
78
#endif
/* ICALLADDRS_H */
79
// end of ICall_Constants
comdef.h
Common Defines.
_icall_remote_task_arg_t
Data type of the first argument passed to the entry point of an image which contains a remote task...
Definition:
icall.h:846
startup_entry
void startup_entry(const ICall_RemoteTaskArg *arg0, void *arg1)
user0Cfg
icall_userCfg_t user0Cfg
user config
icall.h
ICall layer interface.
© Copyright 1995-2025
, Texas Instruments Incorporated. All rights reserved.
Trademarks
|
Privacy policy
|
Terms of use
|
Terms of sale