TI BLE5-Stack API Documentation  9.14.00
Macros | Functions | Variables
icall_addrs.h File Reference

Detailed Description

Stack image address information specific to build.

Go to the source code of this file.

Macros

#define ICALL_ADDR_MAPS
 
#define ICALL_CUSTOM_INIT_PARAMS   { USER0_CFG }
 
#define ICALL_TASK_STACK_SIZES   { 1500 }
 
#define USER0_CFG   &user0Cfg
 user config More...
 

Functions

void startup_entry (const ICall_RemoteTaskArg *arg0, void *arg1)
 

Variables

icall_userCfg_t user0Cfg
 user config More...
 

Macro Definition Documentation

§ ICALL_ADDR_MAPS

#define ICALL_ADDR_MAPS
Value:
{ \
}
void startup_entry(const ICall_RemoteTaskArg *arg0, void *arg1)
void(* ICall_RemoteTaskEntry)(const ICall_RemoteTaskArg *arg0, void *arg1)
Service entry function prototype.
Definition: icall.h:863

Function Documentation

§ startup_entry()

void startup_entry ( const ICall_RemoteTaskArg arg0,
void *  arg1 
)

Initializer for an array of ICall_RemoteTaskEntry. Each element of the array corresponds to an entry function of an external image.

Variable Documentation

§ user0Cfg

icall_userCfg_t user0Cfg

user config

© Copyright 1995-2025, Texas Instruments Incorporated. All rights reserved.
Trademarks | Privacy policy | Terms of use | Terms of sale