TI BLE5-Stack API Documentation  9.14.00
Modules | Data Structures | Typedefs
ATT / GATT Stuctures

Modules

 ATT / GATT Events
 

Data Structures

struct  attAttrBtType_t
 Attribute Type format (2-octet Bluetooth UUID). More...
 
struct  attAttribute_t
 GATT Attribute format. More...
 
struct  attAttrType_t
 Attribute Type format (2 or 16 octet UUID). More...
 
union  attMsg_t
 ATT Message format. More...
 
struct  attPacket_t
 Attribute Protocol PDU format. More...
 
struct  cccValues_t
 CCC Data structure. More...
 
struct  gattAttrType_t
 GATT Attribute Type format. More...
 
struct  gattClientSecCBs_t
 GATT Structure for client security callbacks. More...
 
struct  gattService_t
 GATT Service format. More...
 

Typedefs

typedef struct attAttribute_t gattAttribute_t
 GATT Attribute format. More...
 
typedef bStatus_t(* pfnGATTBondInfoCB_t) (uint16_t connHandle, uint8_t *pMitmReq, uint8_t *pKeySize)
 
typedef bStatus_t(* pfnGATTStartEncCB_t) (uint16_t connHandle)
 

Detailed Description

Typedef Documentation

§ gattAttribute_t

GATT Attribute format.

Note
The list must start with a Service attribute followed by all attributes associated with this Service attribute.

§ pfnGATTBondInfoCB_t

typedef bStatus_t(* pfnGATTBondInfoCB_t) (uint16_t connHandle, uint8_t *pMitmReq, uint8_t *pKeySize)

§ pfnGATTStartEncCB_t

typedef bStatus_t(* pfnGATTStartEncCB_t) (uint16_t connHandle)
© Copyright 1995-2025, Texas Instruments Incorporated. All rights reserved.
Trademarks | Privacy policy | Terms of use | Terms of sale