Changelog

Table of Contents

 

New Features

BLE Stack

ID Summary
BLE_LOKI-3603 Add support for LP-EM-C2755R10-BG for BLE examples
BLE_LOKI-3600 Allow Configuration of Number of Thread Priorities with BLE Thread Defaulting to Highest Priority
BLE_LOKI-1945 L2CAP to Signal application When Peer sends L2CAP Credits

TI Proprietary RF

ID Summary
None None

TI Zigbee

ID Summary
TI_ZIGBEE-263 Add support for application callbacks on start and end of TX and RX operations
TI_ZIGBEE-262 Enable minimum OTA block requests delays less than 50ms
TI_ZIGBEE-255 Enable pre-installed network on Zigbee Rev22
ID Summary
SCCM-606 Enable NVOCMP voltage check for CC23XX and CC27XX
SCCM-585 Add SCCM Examples for LP_EM_CC2755R10_BG

Core SDK

ID Summary
TIDRIVERS-7497 CAN: Implement workaround for errata SYS_211
TIDRIVERS-7492 Enable Secure Debug Manager in SysConfig for CC27XX Family
TIDRIVERS-7452 APU: Implement workaround for errata SYS_211
LPRFXXWARE-1062 APU: Deprecate functions due to errata SYS_211

Radio Control Library (RCL)

ID Summary
RCL-1085 BLE CS: Make the NSTEPS configurable during runtime

 

Fixed Issues

BLE Stack

ID Summary
BLE_LOKI-3773 ICALL Thread Task Priority Adjustment
BLE_LOKI-3768 Timer Double Abort Potential Issue within Car Node Example Project
BLE_LOKI-3757 Connection handover data size is abnormally large on SDK 9.14
BLE_LOKI-3755 Channel Sounding Repetition Termination Mechanism Fixes
BLE_LOKI-3723 Wrong Result Format due to Memory Corruption when using Channel Sounding Repeat Procedures
BLE_LOKI-3716 Channel Sounding Procedure Enable Fails for Coded Phy in all Modes
BLE_LOKI-3657 Unexpected Behavior in First Channel Sounding Distance Events Following Reconnection
BLE_LOKI-3330 Channel Sounding Procedure Repetition Termination is not supported
BLE_LOKI-3224 CS TPM is limited to 40us and offset is increased to 1.5ms
BLE_LOKI-3209 Potential Memory Leak while Running Fuzz Test with L2CAP Connection, Configuration and Disconnection Packets
BLE_LOKI-3172 L2CAP Channel is not established after connection is handed over backwards, when devices are not Paired
BLE_LOKI-3154 Channel Sounding Procedure Repetitions stops if connection event fails

TI Proprietary RF

ID Summary
None None

TI Zigbee

ID Summary
TI_ZIGBEE-260 Hardcoded 50ms delay between fragmented packets
ID Summary
SCCM-608 Compaction bug that results in items lost

Core SDK

ID Summary
TIDRIVERS-7542 Race condition can cause erroneous message lost when handling Rx FIFO in CAN driver
TIDRIVERS-7518 ClockP_scheduleNextTick() does not correctly clear event caused by the previous compare value
TIDRIVERS-7495 APULPF3_polarToCartesianVector accesses object.result before it is initialized
LPRFXXWARE-1071 Increase number of synchronization cycles after writes to APU from 2 to 4 due to errata SYS_211
LPRFXXWARE-1070 Ensure APU registers with side effects are handled correctly due to errata SYS_211
LPRFXXWARE-1063 Ensure read and write consistency to APU registers and program memory due to errata SYS_211
LPRFSEC-237 HSM Crypto Drivers deadlock with KeyStore operations

Radio Control Library (RCL)

ID Summary
None None

 

Known Issues

BLE Stack

ID Summary
BLE_LOKI-3724 IAR Compiler Error when Compiling Basic_persistent on CC2340 Devices
BLE_LOKI-3676 Channel Sounding Timeout Distance Events for Mode 3 with 2x2 Antennas
BLE_LOKI-3536 If parameter update or channel map update w/ CSA#1 is from the past - Connection Monitor will terminate
BLE_LOKI-3535 Connection Monitor Cannot properly track connection on Coded PHY
BLE_LOKI-3473 IAR Compiled Car Node and Key Node Executing Channel Sounding in Loops Causes GAP Link Termination
BLE_LOKI-3429 No Distance is Received after 160 to 255 CS Procedures using RAS over Indications
BLE_LOKI-3389 CS procedure must be complete before starting the next one
BLE_LOKI-3236 Calling HCI_ResetCmd Causes Program to Crash
BLE_LOKI-3208 BLE Agent GUI not able to calculate time offset correctly when running connection handover demo which causes frequent unsuccessful handover sessions
BLE_LOKI-3177 [SWAT] Observer failed to receive GAP_EVT_SCAN_DISABLED event
BLE_LOKI-3097 After changing PHY both devices continue to send Power Reporting events
BLE_LOKI-2978 Connnection Handover AuthenticationComplete Event Received after Handover When Candidate Configured To Initiate Pairing Request
BLE_LOKI-2842 CC23XX and CC27XX family of devices rounds down Tx power values that are not in the power table
BLE_LOKI-2650 CC2745R10Q1 Central Role Fails to Switch Connection PHY to Coded While Holding 16 Connections
BLE_LOKI-2648 Connection may be unstable with Coded PHY when Access Address has high cross-correlation with the preamble
BLE_LOKI-2373 CC2340R5 MAX periodic adv list size is hard coded and can't be configure by SysConfig
BLE_LOKI-2358 CC2340R5 Basic MR printed peripheral initial RPA after bond and pair, instead of its Public Address
BLE_LOKI-2108 Specific smart phone doesn't find peer running extended ADV with secondary PHY of 1M
BLE_LOKI-1630 Extended Advertisement Reports Are Not Filtered When SCAN_PARAM_FLT_DUP is Enabled

TI Proprietary RF

ID Summary
None None

TI Zigbee

ID Summary
None None
ID Summary
None None

Core SDK

ID Summary
TIDRIVERS-7475 I2S driver may not be used simultaneously with CAN or APU driver
TIDRIVERS-7416 The Power driver does not handle SysTimer channel 5 for CC27XX
TIDRIVERS-7244 Changing the muxing on an IO can cause glitches under some conditions
TIDRIVERS-7234 FPU registers not saved/restored around standby for NoRTOS/CM33
TIDRIVERS-7016 AESCCM/AESGCM driver do not support segmented finalize with no input when using HSM engine for CC27XX devices
TIDRIVERS-6863 JSON library unstable for gcc 12.3

Radio Control Library (RCL)

ID Summary
RCL-343 PBE NESB - Address mismatch counter not implemented