SimpleLink™ CC2340R53-Q1 LaunchPad™ Settings & Resources
The SimpleLink™ CC2340R53-Q1 LaunchPad™ contains a CC2340R53E0WRHBRQ1 device.
Jumper Settings
- Close the
LEDsjumpers to enable the on-board LEDs. - Close the
SCLjumper to enable I2C SCL or theBTN1jumper to enable Button 1. These two jumper settings are mutually exclusive. - Close the
SDAjumper to enable I2C SDA or theBTN2jumper to enable Button 2. These two jumper settings are mutually exclusive.
SysConfig Board File
The LP_EM_CC2340R53_Q1.syscfg.json is a handcrafted file used by SysConfig. It describes the physical pin-out and components on the LaunchPad.
Driver Examples Resources
Examples utilize SysConfig to generate software configurations into the ti_drivers_config.c and ti_drivers_config.h files. The SysConfig user interface can be utilized to determine pins and resources used. Information on pins and resources used is also present in both generated files.
TI BoosterPacks™
The following BoosterPacks are used with some driver examples.
BOOSTXL-SHARP128 LCD & SD Card BoosterPack
- BoosterPack pin header BP.8 (
SD_CS) must be jumpered to BP.27 when using the SD card.
BP-BASSENSORSMKII BoosterPack
The TMP116’s power pin is not compatible with this LaunchPad. Use the following modification to enable the TMP116’s usage with the i2ctmp and portable examples.
- Use a jumper wire to connect BoosterPack pin header BP.28 (
T_V+) to BP.1 (3V3).
The OPT3001’s interrupt pin is not compatible with this LaunchPad. Use the following modification to enable the OPT3001’s usage with the i2copt3001_cpp example.
- Use a jumper wire to connect BoosterPack pin header BP.25 (
O_INT) to BP.7 (unlabeled).
CC3200 Audio BoosterPack
- No modifications are needed.
BP-EM-CS BoosterPack
When using a CC23X0 board, connect the P3 and P4 jumpers, and disconnect the P1 and P2 jumpers on the BoosterPack. Add only the VC pins labelled CC23X0 in SysConfig and make sure they are configured as output.
The VC pins are used to select the antenna on the BoosterPack:
| RF1 (J2) | RF2 (A1) | RF3 (A2) | RF4 (J3) | |
|---|---|---|---|---|
| VC1 | 0 | 0 | 1 | 1 |
| VC2 | 0 | 1 | 0 | 1 |