#-------------------------------------------------------------------------------
# Copyright (c) 2022-2023, Arm Limited. All rights reserved.
#
# SPDX-License-Identifier: BSD-3-Clause
#
#-------------------------------------------------------------------------------

mainmenu "TF-M Configuration"

# Load platform Kconfig file if exists
osource "$(PLATFORM_PATH)/Kconfig"
osource "$(TFM_SOURCE_DIR)/config/build_type/Kconfig.$(CMAKE_BUILD_TYPE)"

################################# System options ###############################

rsource "Kconfig.bl"
rsource "secure_fw/spm/Kconfig"
rsource "secure_fw/partitions/Kconfig" # These are partition switches.
rsource "platform/Kconfig"
rsource "Kconfig.misc"

################################# Test options #################################

menu "TF-M tests"
rsource "lib/ext/tf-m-tests/Kconfig"
rsource "lib/ext/psa_arch_tests/Kconfig"
endmenu

################################# Component ####################################

# These configs in this menu are local to a component or externally referenced
# when components are coupled. Usually, such options are located in C header
# file. The Header File Config System has more details about it.

# Other configs above which are not in component menu are TF-M build options to
# select which file or component to include into compilation. These are options,
# usually used by a build system to enable/disable modules, specify location of
# external dependency or other selection, global to a project. These options
# shall be considered while adopting TF-M to other build systems.

menu "TF-M component configs"

# Load configurations set by PSA arch test
if TEST_PSA_API != ""
    rsource "$(TFM_SOURCE_DIR)/config/tests/Kconfig.test_psa_api"
endif

rsource "secure_fw/spm/Kconfig.comp"

menu "Secure Partitions component configs"
    rsource "secure_fw/partitions/*/Kconfig.comp"
endmenu
endmenu