Example Summary
This example shows how to use the Non-Volatile Storage (NVS) driver to read and write data to on-chip flash memory.
Peripherals & Pin Assignments
When this project is built, the SysConfig tool will generate the TI-Driver configurations into the ti_drivers_config.c and ti_drivers_config.h files. Information on pins and resources used is present in both generated files. Additionally, the System Configuration file (*.syscfg) present in the project may be opened with SysConfig’s graphical user interface to determine pins and resources used.
CONFIG_NVSINTERNAL- Non-volatile storage used by a NVS driver instance.
BoosterPacks, Board Resources & Jumper Settings
For board specific jumper settings, resources and BoosterPack modifications, refer to the Board.html file.
If you’re using an IDE such as Code Composer Studio (CCS) or IAR, please refer to Board.html in your project directory for resources used and board-specific jumper settings.
The Board.html can also be found in your SDK installation:
<SDK_INSTALL_DIR>/source/ti/boards/<BOARD>
Example Usage
Example output is generated through use of Display driver APIs. Refer to the Display driver documentation.
- Open a serial session (e.g.
PuTTY, etc.) to the appropriate COM port.- The COM port can be determined via Device Manager in Windows or via
ls /dev/tty*in Linux.
- The COM port can be determined via Device Manager in Windows or via
The connection will have the following settings:
Baud-rate: 115200
Data bits: 8
Stop bits: 1
Parity: None
Flow Control: None
Run the example.
The example will output the region attributes as defined by
CONFIG_NVSINTERNAL.- The example checks if the string, “SimpleLink SDK Non-Volatile Storage (NVS) Example” is present in non-volatile storage.
- If present, the string is displayed to the UART console. The entire flash sector is then erased.
- If not present, the string is written to the non-volatile storage.
Disconnect the device from the debug session.
When prompted, reset the device. This will cause the application to start over.
The region base address, sector size and region size will vary depending on the device.
NOTE FOR GCC: Sysconfig is not able to place the NVS region at the address specified by the “Region Base” configuration parameter (0x10000 in this example). If your application requires the NVS region to begin at a specific location, the linker script must be modified to explicitly place the .nvs section at the desired address. For example to place the .nvs section at 0x10000, the .nvs section should look as follows:
SECTIONS: {
...
.nvs 0x10000 (NOLOAD) : ALIGN(0x2000) {
*(.nvs)
} > REGION_TEXT
...
}
The following is example output assuming the string was not present in non-volatile storage:
Region Base Address: 0x1B000
Sector Size: 0x1000
Region Size: 0x4000
Writing signature to flash...
Reset the device.
==================================================
The following is example output assuming the string is present in non-volatile storage:
Region Base Address: 0x1B000
Sector Size: 0x1000
Region Size: 0x4000
SimpleLink SDK Non-Volatile Storage (NVS) Example.
Erasing flash sector...
Reset the device.
==================================================
Application Design Details
The application utilizes a single thread to demonstrate using the non-volatile storage region defined by
CONFIG_NVSINTERNAL.CONFIG_NVSINTERNALdefines a non-volatile storage located on the device’s on-chip internal flash memory. The memory definitions may be found in the board file. AfterNVS_open(), thenvsHandleis associated with the memory region defined byCONFIG_NVSINTERNAL.- A block of memory the size of
signaturebytes is read from flash and copied into RAM (buffer). An offset of 0 is used with theNVS_read()call. The NVS memory location read is therefore equal to the NVS region base address,NVS_Attrs.baseAddress. The contents copied intobufferare compared tosignature.- If equal, the application displays the signature to the UART console. It is important to note that the string was copied into RAM (
buffer) duringNVS_read(). This example chooses to display the string directly from the NVS region in flash. After the string is output to the UART console, the first sector in the NVS region is erased. - If not equal, the application writes the string,
signatureto the NVS region. An offset of 0 is specified with theNVS_writecall. The NVS memory location written to is therefore equal to the NVS region base address,NVS_Attrs.baseAddress.
- If equal, the application displays the signature to the UART console. It is important to note that the string was copied into RAM (
At the end of execution, the application prompts the user to reset the device. Upon a reset, the contents of volatile memory (RAM) are lost. The example application restarts.
The
NVS_WRITE_ERASEflag is used with theNVS_write()API to ensure the flash sector is erased prior to performing a write. This flag will eraseNVS_Attrs.sectorSizebytes of memory starting at the offset specified withNVS_write().The
NVS_WRITE_POST_VERIFYflag is also used with theNVS_write()API to ensure the flash memory was successfully written.
FreeRTOS:
- Please view the
FreeRTOSConfig.hheader file for example configuration information.