MCUboot Over-the-Air Download (OAD)¶
The following sections aim to describe the lower layers of OAD software that are common across all protocol stack implementations. This includes the OAD image header, the flash layout, Secure Bootloader, and the oad image tool.
The following sections aim to describe the Zigbee 3.0 specific application and profile layer of the OAD solution. The OAD application section will describe the Zigbee OAD process from a high level in terms of events and states, and the profile section will cover the actual structures that are sent over the air.