Disable SysConfig

This section will describe the steps necessary to disable SysConfig, either entirely or just a few selected files.Disabling SysConfig may be necessary when freezing source code for production or when you are satisfied with the output.

This example will use the simple_peripheral project from the BLE5-Stack, but the steps can be adopted for project.

A summarization of the steps can be found below:

  1. Build the project at least once so that SysConfig can generate output

  2. Locate the generated files

  3. Copy generated files from build directory

  4. Modify compiler/linker files to point to moved files

  5. Stop SysConfig from running by either:

    1. Excluding generated files from building.

    2. Changing the .cproject file and disabling the pre-build step

Tip

Check if configuring SysConfig to Reserve Peripheral(s) could help.

Locating Generated Files

After building the simple_peripheral project using default settings, the first step to disabling SysConfig is to determine which files it has generated.

Click the <> button in SysConfig to see which files it is currently generating. See SysConfig generated files for an example of which files are generated by SysConfig for the simple_peripheral project.

In CCS these files are placed in <build_config>/syscfg

  • <build_config> is the build configuration of the project. (e.g. Debug)

In IAR these files are placed in the project folder (e.g. ~/<proj_import>/)

  • <proj_import> is the location selected when importing the project in IAR

  • In the IDE the SysConfig files reside in a virtual folder called SysConfig Generated Files. You can find their location by right clicking any of the files in this folder and selecting “Open Containing folder…”

../_images/generated_files_sp.png

SysConfig generated files. Command files are marked with yellow.

Copy Generated Files

IAR Users may skip this step

In CCS the build directory is cleaned every time the project is rebuilt, so it is necessary to copy the generated files to a permanent location before the project is rebuilt. Follow the steps below to do so. We will place the files in the application in a folder called syscfg but it can be called anything.

  1. Right click on the project -> New -> Folder

  2. Copy the files from <build_config>/syscfg to the new folder.

Attention

When debugging using ROV, be sure to place syscfg_c.rov.xs in the root directory of the project. This way, the ROV tool can pull in the appropriate debug tools as selected by SysConfig initially.

Modifying Compiler/Linker Settings

IAR Users may skip this step as the SysConfig output is already in a non destructive location. However, if you moved the SysConfig generated content to a new location elsewhere in the file system, you may need to change the project settings.

The .c, .h, and .opt files generated by SysConfig are consumed by the compiler and linker as part of the build process. Moving the files to a new location means that we need to modify the project settings to find them. For the case of simple_peripheral this means:

  1. Change include paths (Project > Properties > ARM Compiler > Include Options)

  • Add ${PROJECT_ROOT}/syscfg

2. Change location of .opt files (Project > Properties > ARM Compiler > Advanced Options > Command Files)

  • Change the location of the ti_build_config.opt and ti_ble_app_config.opt to be in ${PROJECT_ROOT}/syscfg

  1. Modify linker include paths (Project > Properties > ARM Linker > File Search Path)

  • Change the location of ti_utils_build_linker.cmd.genlibs from ${PROJECT_BUILD_DIR}/syscfg/ to be in ${PROJECT_ROOT}/syscfg/

First method: Excluding Generated Files from Building

This method is recommended if users only want to modify some of the .c/h files which are generated, but not stop Sysconfig from running during a project build. In order to do this, click the <> button in SysConfig and deselect the Include in Build button of files you no longer want generated by SysConfig. Make sure that these files are the only ones which have been copied into your custom syscfg application folder.

../_images/exclude_generated_files_sp.png

SysConfig generated files, excluded ones of which have been deselected.

Second method: Stop SysConfig from Running Entirely

The following steps are required to completely remove SysConfig’s involvement during a project build.

  1. Open the .cproject file.

../_images/cproject_file.png

Find the .cproject file.

  1. In this file, find and comment out or remove the XML element <tool name="SysConfig"/>, as shown below:

. . .
</tool>
<tool id="com.ti.ccstudio.buildDefinitions.TMS470_20.2.hex.1150171138" name="ARM Hex Utility" superClass="com.ti.ccstudio.buildDefinitions.TMS470_20.2.hex"/>
<!--tool id="com.ti.ccstudio.buildDefinitions.sysConfig.752181800" name="SysConfig" superClass="com.ti.ccstudio.buildDefinitions.sysConfig">
  <option IS_BUILTIN_EMPTY="false" IS_VALUE_EMPTY="false" id="com.ti.ccstudio.buildDefinitions.sysConfig.PRODUCTS.967104601" name="Root system config meta data file in a product or SDK (-s, -/-product)" superClass="com.ti.ccstudio.buildDefinitions.sysConfig.PRODUCTS" useByScannerDiscovery="false" valueType="stringList">
    <listOptionValue builtIn="false" value="${COM_TI_SIMPLELINK_CC13XX_26XX_SDK_SYSCONFIG_MANIFEST}"/>
  </option>
</tool-->
<tool id="com.ti.rtsc.buildDefinitions.XDC_3.16.tool.499843531" name="XDCtools" superClass="com.ti.rtsc.buildDefinitions.XDC_3.16.tool">
. . .

Note 1: Make sure that you also break-up any double dashes inside that commented out XML section (e.g. see the string -/-product above, which used to be --product).

Note 2: Make sure that you comment out the <tool> element which is inside the (build) <configuration> element for which you wish to disable the SysConfig tool. I.e. build config Debug or Release.

  1. Open the Project Explorer view’s menu (the triple dot icon in the top-right corner of the Project Explorer view), and open the Filters and Customization… dialog.

  2. In the dialog, de-select the .* resources entry (second entry from the top), and click OK.

After applying these steps, SysConfig will no longer run (and it will not show up in the Project overview). To remove SysConfig entirely, the build step must be removed as well. Disabling SysConfig is slightly different for IAR vs CCS. Expand the relevant section below to see how to disable SysConfig.

Click to IAR Instructions

In IAR, SysConfig is treated as a Custom Build step. To access the custom build steps select Project > Options > Custom Build. Remove all the fields that are populated under the Custom Tool Configuration tab as shown below:

../_images/sysconfig-disable-iar.png

Disable SysConfig IAR

Click to CCS Instructions

In CCS, files ending in .syscfg are automatically flagged as SysConfig files. If you have a file active in your workspace, it will invoke the SysConfig tool. This can be disabled by excluding the .syscfg files from build.