Disable SysConfig¶
This section will describe the steps necessary to disable SysConfig, either entirely or just a few selected files. Disabling SysConfig may be necessary when freezing source code for production or when you are satisfied with the output.
This example will use the basic_ble project from the BLE5-Stack,
but the steps can be adopted for other project.
A summarization of the steps can be found below:
Build the project at least once so that SysConfig can generate output
Locate the generated files
Copy generated files from build directory
Modify compiler/linker files to point to moved files
Exclude generated files from build:
Optional: Exclude .syscfg from build
Locating Generated Files¶
After building the basic_ble project using default settings, the first
step to disabling SysConfig is to determine which files it has generated.
Click the <> button in SysConfig to see which files it is currently
generating. See SysConfig generated files for an example of which files
are generated by SysConfig for the basic_ble project.
In CCS these files are placed in <build_config>/syscfg
<build_config>is the build configuration of the project. (e.g.Debug)
In IAR these files are placed in the project folder (e.g. ~/<proj_import>/)
<proj_import>is the location selected when importing the project in IARIn the IDE the SysConfig files reside in a virtual folder called SysConfig Generated Files. You can find their location by right clicking any of the files in this folder and selecting Open Containing folder…
Figure 78. SysConfig generated files¶
Copy Generated Files¶
IAR Users may skip this step
In CCS the build directory is cleaned every time the project is rebuilt,
so it is necessary to copy the generated files to a permanent location
before the project is rebuilt. Follow the steps below to do so. We will
place the files in the application in a folder called syscfg but it
can be called anything.
Right click on the project -> New -> Folder
Copy the files from
<build_config>/syscfgto the new folder.
See Generated Files to see which files to copy. Note that the .syscfg file should not be moved.
Attention
When debugging using ROV, be sure to place syscfg_c.rov.xs in the root
directory of the project. This way, the ROV tool can pull in the appropriate
debug tools as selected by SysConfig initially.
Modifying Compiler/Linker Settings¶
IAR Users may skip this step as the SysConfig output is already in a non destructive location. However, if you moved the SysConfig generated content to a new location elsewhere in the file system, you may need to change the project settings.
The .c, .h, and .opt files generated by SysConfig are consumed
by the compiler and linker as part of the build process. Moving the files
to a new location means that we need to modify the project settings to
find them. For the case of basic_ble this means:
Change include paths (Project > Properties > ARM Compiler > Include Options)
Add
${PROJECT_ROOT}/syscfg
2. Add .opt file path. You may skip this step if you do not want to exclude the .opt file from SysConfig.
(Project > Properties > ARM Compiler > Advanced Options > Command Files)
Add the path of the
ti_utils_build_compiler.optfile:${PROJECT_ROOT}/syscfg/ti_utils_build_compiler.opt
3. Add linker include path (Project > Properties > ARM Linker > File Search Path) You may skip this step if you do not want to exclude the .genlibs file from SysConfig.
Add the directory
${PROJECT_ROOT}/syscfg/so that the linker can find the fileti_utils_build_linker.cmd.genlibs
Exclude Generated Files from Build¶
In order to do this, click the <> button in SysConfig and deselect the
Include in Build button of files you no longer want generated by SysConfig.
Make sure that these files are the only ones which have been copied into your
custom syscfg application folder.
Figure 79. SysConfig generated files, excluded ones of which have been deselected.¶
Optional: Exclude .syscfg from build¶
The following step is required to completely remove SysConfig’s involvement during a project build.
Right click on the .syscfg file. Select the option “Exclude from build”.
Note
Your project will not compile unless either you copied all the SysConfig generated files or
write your own code with the necessary defines and initializations.