|SDK| Overview
$$$$$$$$$$$$$$$$$$$$$$$

The SimpleLink\ |trade| |DEVICEAND| Software Development Kit provides a
complete package for the development of Bluetooth LE, PropRF, and Zigbee, 
applications for the |DEVICE| wireless microcontroller.

Introduction to the |SDK|
#########################

.. Copied from product page (http://www.ti.com/tool/launchxl-cc26x2r1)

TI's royalty-free |SDK| is a complete software platform for developing
applications that require low-power, security, reliability, and mesh
networking. The |DEVICEAND| devices are part of the SimpleLink\ |trade| MCU
platform which consists of Wi-Fi\ |reg|, Bluetooth\ |reg| Low Energy, Sub-1 GHz,
Thread, Zigbee, IEEE 802.15.4 and host MCUs, which all share a common, easy-to-use
development environment and rich tool set. A one-time integration of the
SimpleLink\ |trade| platform enables you to add any combination of the
portfolio's devices into your design, allowing 100 percent code reuse when
your design requirements change. For more information, visit the
`SimpleLink™ Solutions Overview
<http://www.ti.com/lsds/ti/wireless-connectivity/simplelink-solutions/overview.page>`_.

Solution Platform
^^^^^^^^^^^^^^^^^

This section describes the various components that are installed with the
|SDK|, the directory structure of the protocol stack, and any tools required
for development.

The following components are included in the solution platform:

- Real-time operating system (|RTOS|), optimized power management support, and 
  peripheral drivers.

- The driverLib provides a register abstraction layer that is used by software
  and drivers to control the |DEVICE| MCU.

- TI-Drivers are a set of RTOS aware drivers designed to allow seemless use of
  |DEVICE| peripherals inside your application.

- Example applications make the beginning stages of development easier. Example
  applications are provided for the |DEVICE| platform


.. _sec-directory-structure:

Directory Structure
-------------------

The |SDK| directory structure is broken down into a few major directories at
the root to allow easy differentiation between documentation, examples, kernel
source, and other source code. From the root directory, the sub-directories
are:

:docs: Contains HTML and PDF documentation for the |SDK|.
:examples: Contains the example projects and example source for this |SDK|.
:kernel: Contains the source and build tools for the kernels supported by this
         |SDK|.
:source: Contains the source code for the larger components of the |SDK|. A
         more detailed description of this directory follows.
:tools: Scripts and definition files used by the |SDK|. Contains scripts
        referenced by the |SDK| documentation.

The source directory is split into major categories based on where the source
code came from. All of the source code within the ``source\third_party`` directory
comes from vendors other than Texas Instruments. All of the source code within
the ``source\ti`` directory comes from Texas Instruments.

:ti\\boards: Contains the board hardware configurations.
:ti\\devices: Contains the board support source code.
:ti\\display: Contains the source code for the display libraries.
:ti\\drivers: Contains the source code for the TI drivers.
:ti\\grlib: Contains the source code for the graphics libraries.