.. _chap-example-applications:

Running the Example Applications
$$$$$$$$$$$$$$$$$$$$$$$$$$$$$$$$

This section provides an overview of the |STACK| out-of-box example
applications and instructions on how to run them.  The examples are out-of-box
compliant with the ZCL v8 Specification but will further :ref:`sec-product-certification`
will be required.

Note: This document references the CC2340R5 example READMEs, although the same 
README locations can be found for any |STACK| compatible |DEVICE| device.

-  :docs_root:`Green Power Attribute Reporting Readme  <../examples/rtos/LP_EM_CC2340R5/zigbee/gpd_attr_reporting/README.html>`: Report attributes using the Green Power Device application

-  :docs_root:`Green Power Bidirectional Read and Write Attributes Readme  <../examples/rtos/LP_EM_CC2340R5/zigbee/gpd_bidir_attr_read_write/README.html>`: Read and write attributes using the Green Power Device application

-  :docs_root:`Green Power Switch Readme  <../examples/rtos/LP_EM_CC2340R5/zigbee/gpd_switch/README.html>`: Control a on/off switch using the Green Power Device application

-  :docs_root:`Light End Device Readme  <../examples/rtos/LP_EM_CC2340R5/zigbee/onoff_light/README.html>`: Control a ZCL on/off light output server

-  :docs_root:`Switch End Device Readme  <../examples/rtos/LP_EM_CC2340R5/zigbee/onoff_switch/README.html>`: Control a ZCL on/off switch client

-  :docs_root:`Off-chip OTA Switch End Device Readme  <../examples/rtos/LP_EM_CC2340R5/zigbee/onoff_switch_ota_client_offchip/README.html>`: Control a ZCL on/off switch client, including off-chip OTA client capabilities

-  :docs_root:`On-chip OTA Switch End Device Readme  <../examples/rtos/LP_EM_CC2340R5/zigbee/onoff_switch_ota_client_onchip/README.html>`: Control a ZCL on/off switch client, including on-chip OTA client capabilities and a OTA candidate image compression feature