Application Overview
====================

|STACK| example applications are designed to enable faster end-product development by
providing different implementations of Zigbee device definitions while conforming to
`ZCL v8 Specifications <https://zigbeealliance.org/wp-content/uploads/2021/10/07-5123-08-Zigbee-Cluster-Library.pdf>`_ 
requirements for certification.  This allows the
developers to explore the usage of the stack for configuring and running a device in
a network along with other essential features, such as nonvolatile (NV) memory storage 
to save the network parameters and application specific information. The configuration 
and usage of peripherals such as switches and LEDs are also shown by these 
sample applications. This chapter explains the application's implementation to help 
developers quickly modify the |STACK| out-of-box example applications for customized 
development. A full description is proviced in the |ZBOSS_UG|.

.. _sec-application-architecture:

Application Architecture
------------------------

:numref:`fig-example-application-block-diagram` shows the block diagram of the
Light and Switch example applications on the |DEVICEAND|. 

.. _fig-example-application-block-diagram:
.. figure:: resources/fig-example-application-block-diagram.png
    :align: center

    Example Application Block Diagram


High-level descriptions of various blocks in :numref:`fig-example-application-block-diagram` 
are as follows:

**FreeRTOS Start-up Code:** Initializes the application (see
:ref:`sec-start-up-in-main` for more
details).

**Example Application:** The platform-independent implementation of the example
use case. The |STACK| out-of-box demonstrates two use cases – Light and
Switch. Developers can modify this module's out-of-box example code for custom
for custom application requirements to quickly develop end products. 

**Utility Functions:** Provides various platform utilities which the application
can use.  Examples include LED, timers, keys, and so on.

**Application-Specific Functions:** Implements platform-specific functions such
as data storage over power cycles (nonvolatile) and provides user interface
functions, such as handling button presses.

**ZBOSS API Module (API ZBOSS Module):** This module provides an interface
to the management and data services of the Zigbee stack.

.. _sec-app-configuration:

Application Preprocessor Configuration
^^^^^^^^^^^^^^^^^^^^^^^^^^^^^^^^^^^^^^

A few preprocessor symbols exist to operate |STACK| within the project. They are \
located in the Project Properties as further discussed in the *Useful CCS IDE 
Settings* section of the |ZB_QUICK_START_GUIDE|.

    .. note:: Please refer to the preprocessor symbols section of the 
        |ZB_QUICK_START_GUIDE| to setup compile options for the project if using IAR.

.. _sec-start-up-in-main:

Start-Up in main()
^^^^^^^^^^^^^^^^^^

The :code:`main()` function inside of :code:`ti_f3_main.c` is the application 
starting point at runtime. This is where the board is brought up with interrupts 
disabled and board-related components are initialized. Tasks in this function 
are configured by initializing the necessary parameters, setting their priority, 
and initializing the stack size for the application. The primary IEEE address 
(programmed by TI) is obtained from the :term:`CCFG` area of the flash memory 
and TI drivers are initialized.  In the final step, the ``FreeRTOS`` scheduler is 
started by calling :code:`vTaskStartScheduler()`, which does not return. See the 
|TRM| for information on the start-up sequence before :code:`main()` is reached.

.. code-block:: c

	int main(void)
	{
	pthread_t           thread;
	pthread_attr_t      attrs;
	struct sched_param  priParam;
	int                 retc;
	int                 detachState;

	/* Call driver init functions */
	Board_init();

	/* Set priority and stack size attributes */
	retc = pthread_attr_init(&attrs);
	if (retc != 0)
	{
		/* pthread_attr_init() failed */
		FATAL_ERR();
	}

	priParam.sched_priority = 1;

	detachState = PTHREAD_CREATE_DETACHED;
	retc = pthread_attr_setdetachstate(&attrs, detachState);
	if (retc != 0)
	{
		/* pthread_attr_setdetachstate() failed */
		FATAL_ERR();
	}

	retc = pthread_attr_setschedparam(&attrs, &priParam);
	if (retc != 0)
	{
		/* pthread_attr_setschedparam() failed */
		FATAL_ERR();
	}

	retc = pthread_attr_setstacksize(&attrs, THREADSTACKSIZE);
	if (retc != 0)
	{
		/* pthread_attr_setstacksize() failed */
		FATAL_ERR();
	}

	retc = pthread_create(&thread, &attrs, main_task_function, NULL);
	if (retc != 0)
	{
		/* pthread_create() failed */
		FATAL_ERR();
	}

	/* Start the FreeRTOS scheduler */
	vTaskStartScheduler(); /* does not return */

	return (0);
	}

In terms of the IDE workspace, ``ti_f3_main.c`` exists in the Application project –
meaning that when compiled it is placed in the allocated section of the application's flash.

.. _sec-application-init-function:

Application Initialization Function
^^^^^^^^^^^^^^^^^^^^^^^^^^^^^^^^^^^

:ref:`FreeRTOS Tasks` describes how a task is constructed. After the
task is constructed and the ``FreeRTOS`` scheduler is started, the function that 
was passed during task construction is run when the task is ready. Specific |STACK| 
functions are called to establish the node processes ans start the device.

.. code-block:: c

	MAIN()
	{
	ARGV_UNUSED;

	/* Trace enable */
	ZB_SET_TRACE_OFF();
	/* Traffic dump enable */
	ZB_SET_TRAF_DUMP_OFF();

	/* Global ZBOSS initialization */
	ZB_INIT("on_off_switch");


	#ifdef ZB_COORDINATOR_ROLE
	/* Set up defaults for the commissioning */
	zb_set_long_address(g_zc_addr);
	zb_set_network_coordinator_role(DEFAULT_CHANLIST);
	zb_secur_setup_nwk_key(g_nwk_key, 0);
	zb_set_max_children(1);

	#elif defined ZB_ROUTER_ROLE && !defined ZB_COORDINATOR_ROLE
	/* Set up defaults for the commissioning */
	zb_set_long_address(g_zr_addr);
	zb_set_network_router_role(DEFAULT_CHANLIST);
	zb_set_max_children(1);

	#elif defined ZB_ED_ROLE
	/* Set up defaults for the commissioning */
	zb_set_long_address(g_zed_addr);
	zb_set_network_ed_role(DEFAULT_CHANLIST);

	/* Set end-device configuration parameters */
	zb_set_ed_timeout(ED_AGING_TIMEOUT_64MIN);
	// zb_set_keepalive_timeout(ZB_MILLISECONDS_TO_BEACON_INTERVAL(3000));
	zb_set_rx_on_when_idle(ZB_TRUE);
	#endif


	zb_set_nvram_erase_at_start(ZB_FALSE);
	/* Register device ZCL context */
	ZB_AF_REGISTER_DEVICE_CTX(&on_off_switch_ctx);
	/* Register cluster commands handler for a specific endpoint */
	ZB_AF_SET_ENDPOINT_HANDLER(ZB_SWITCH_ENDPOINT, zcl_specific_cluster_cmd_handler);

	/* Initiate the stack start without starting the commissioning */
	if (zboss_start_no_autostart() != RET_OK)
	{
		TRACE_MSG(TRACE_ERROR, "zboss_start failed", (FMT__0));
	}
	else
	{
		/* Call the application-specific main loop */
		my_main_loop();
	}

	/* Deinitialize trace */
	TRACE_DEINIT();

	MAIN_RETURN(0);
	}

For application examples, :code:`MAIN` calls :code:`ZB_INIT()`,
which later calls :code:`zb_init` that serves as the entrance for 
the application code to configure |STACK| network parameters as well as 
application specific peripherals configurations, callbacks, and stack 
notifications.

.. _sec-event-processing-task-function:

Event Processing in the Task Function
^^^^^^^^^^^^^^^^^^^^^^^^^^^^^^^^^^^^^

After initializing the peripherals and configuring the application and
implementing the initialization function from the previous code snippet,
:code:`MAIN()`, it enters an infinite loop :code:`my_main_loop` so as to 
continuously process as an independent task and not run to completion, seen 
in :numref:`fig-switch-task-flow-chart`.

.. _fig-switch-task-flow-chart:
.. uml::
    :align: center
    :caption: Switch Example Application Task Flow Chart

    @startuml
    :MAIN();
    :ZB_INIT()]
    :my_main_loop()]
        repeat
        while(Process Zigbee messages)
        :Process Application peripheral events]
        :Process Application events]
        endwhile (No events to process)
        repeat while
    :End;
    @enduml

:numref:`fig-switch-task-flow-chart` shows various reasons for posting to the
semaphore, causing the task to become active.

.. _sec-events-signaled-through-internal-event-variable:

Events Signaled Through the Internal Event Variable
^^^^^^^^^^^^^^^^^^^^^^^^^^^^^^^^^^^^^^^^^^^^^^^^^^^

The :code:`zboss_signal_handler` function uses definitions to identify what action
caused the process to wake up and take appropriate action. The values correspond 
to a defined event such as (not a comprehensive list):

.. code-block:: c

	// Application Events
	#define ZB_ZDO_SIGNAL_SKIP_STARTUP            1U
	#define ZB_ZDO_SIGNAL_DEVICE_ANNCE            2U
	#define ZB_ZDO_SIGNAL_LEAVE                   3U
	#define ZB_ZDO_SIGNAL_ERROR                   4U
	#define ZB_BDB_SIGNAL_DEVICE_FIRST_START      5U
	#define ZB_BDB_SIGNAL_DEVICE_REBOOT           6U
	#define ZB_BDB_SIGNAL_STEERING                10U
	#define ZB_COMMON_SIGNAL_CAN_SLEEP            13U
	#define ZB_ZDO_SIGNAL_PRODUCTION_CONFIG_READY 23U
	#define ZB_BDB_SIGNAL_TC_REJOIN_DONE          58U

These allow for action to be taken at the time each event occurs.

.. _sec-callbacks:

Callbacks
^^^^^^^^^

The application code also likely includes various callbacks from the protocol
stack layer and |RTOS| modules. These have been registered during the 
:code:`MAIN` or :code:`zboss_signal_handler` functions.  Examples include 
:code:`finding_binding_cb`, :code:`zcl_specific_cluster_cmd_handler`, 
:code:`button_press_handler`, and :code:`permit_joining_cb`.

Buttons
^^^^^^^

The basic common user interface controls the funtionality of a push button which 
is already incorporated into the example applications for use with the LaunchPad 
boards:

-   BTN-1: Application-specific function (ex. onoff switch)

More DIOs can be added to fit the requirements of a custom board design and
specific application in accordance with SysConfig initialization, for more
information refer to :ref:`sysconfig-board-files`