.. _creating_custom_ble_app:

*******************************************
Developing with SimpleLink Low Power F3 SDK
*******************************************

The following are additional development resources to assist users with 
integrating the |SDK| into their application environment.

.. _sect-custom-hardware:

==================================
Running the SDK on Custom Hardware
==================================

.. toctree::
   :maxdepth: 1

   /cc23xx/custom-hardware-cc23xx

=====================
Development Resources
=====================
.. toctree::
   :maxdepth: 1

   /cc23xx/gpio-cc23xx.rst
   /cc23xx/timer-cc23xx.rst
   /cc23xx/uart2_dynamic_pin_switching.rst
   /cc23xx/disable-external-flash-cc23xx.rst
   /cc23xx/command-line-flashing-cc23xx.rst
   /cc23xx/enable-s2r-ram-cc23xx.rst
   /cc23xx/system-reset-cc23xx.rst