.. _sec-freertos-software-timers:

Software Timers
---------------

FreeRTOS includes a mechanism called Software Timers that is very similar to
what other RTOS call 'Clocks'. In this section we will provide a brief 
introduction to FreeRTOS Software Timers. For all the details, please visit 
|FreeRTOS SOFTWARE TIMERS| and the |FreeRTOS API|.

The basics
^^^^^^^^^^

A Software Timer allows you to execute a function some time in the future. To
make use of this feature, you will need to:

- Create a software timer

- Define the software timer's callback function (i.e. the function that you
  want to execute in the future)

- Define the software timer's period (i.e. the point in the future when you
  want it executed)

.. warning::

  As indicated in |FreeRTOS SOFTWARE TIMERS|, it is imperative that
  a timer's callback does not attempt to block. That is, it cannot call
  vTaskDelay(), vTaskDelayUntil(), or specify a non-zero block time when
  accessing a queue or a semaphore.

You can select a Software Timer to be one-shot or auto-reload during creation. 
See more details about this in section :ref:`sec-freertos-create-sw-timer-listing` 
below. You may also want to check the FreeRTOS documentation, specifically 
|FreeRTOS SOFTWARE TIMERS ONESHOT VS AUTORELOAD| and the description of
|FreeRTOS xTaskCreate|.

Using Software Timers
^^^^^^^^^^^^^^^^^^^^^

Please note that Software Timers are not part of the core FreeRTOS kernel.
In order to use them, you must first take the following two steps:

#. Add the FreeRTOS/Source/timers.c source file to your project, and...
#. Define a few constants in the FreeRTOSConfig.h header file. 

FreeRTOSConfig.h is part of the freertos_builds project.

See all the details at |FreeRTOS SOFTWARE TIMERS CONFIG|.

Details on Implementation
^^^^^^^^^^^^^^^^^^^^^^^^^

FreeRTOS Software Timers are provided by a timer service (or daemon) task.
Your application will interact with FreeRTOS Timers through API functions,
which will allow you to do operations such as create a timer, start and stop 
a timer, etc. 
These functions use a standard FreeRTOS queue to send commands to the timer 
service task. This queue is called the 'timer command queue' and cannot be
accessed directly. 
Learn more about this at |FreeRTOS SOFTWARE TIMERS SERVICE TASK|.

.. _sec-freertos-create-sw-timer-listing:

Creating and Starting a Software Timer
^^^^^^^^^^^^^^^^^^^^^^^^^^^^^^^^^^^^^^

In this section we will provide an example of how to create and start a
Software Timer. See more examples of usage in the |FreeRTOS API|.

.. code-block:: c
    :linenos:
    :caption: Create a FreeRTOS Software Timer

    #include <FreeRTOS.h>
    #include <stdarg.h>


    TimerHandle_t xTimer;

    void main( void ) {

        BaseType_t xReturned;

        /* Create and start the timer. Recommended to do before starting the scheduler */
        xTimer = xTimerCreate(
                "Timer 1",                      /* Textual name, helpful during debugging! */
                pdMS_TO_TICKS( 500 ),           /* Timer period: 500 ms */
                pdTRUE,                         /* Autoreload */
                ( void * ) 1,                   /* Timer ID. Can be used to identify which
                                                   timer expired if multiple timers share a
                                                   timer callback */
                &vTimerCallback );              /* Function to call when timer expires. When
                                                   invoked by FreeRTOS, the Timer ID will be 
                                                   passed as a parameter */

        if(xTimer != NULL)
        {
            BaseType_t started;
            started = xTimerStart(
                   xTimer,                      /* Handle returned by xTimerCreate */
                   0);                          /* Time to block in ticks: 0 (Do not block) */
            if (pdPASS != sarted) {
                /* Failed to start the timer! */
            }
         } else {
           /* Failed to create the timer! */
         }

        /* Start the FreeRTOS scheduler */
        vTaskStartScheduler();
    }

    /* Timer Callback Function (this may be reused by multiple timers if desired) */
    void vTimerCallback( TimerHandle_t xTimer )
    {
        /* *** Enter your application code here *** */
        /* Ex. */
        static uint32_t timer_count__500ms = 0;
        timer_count__500ms++;
    }