.. _sec-freertos-migration:

Migrating TI-RTOS examples to use FreeRTOS
------------------------------------------

There are significant project setting modifications required to migrate from a
TI-RTOS example to one that supports FreeRTOS, such as modifying the toolchain,
adding include paths, and managing predefined symbols. For this reason, the
recommended approach to port an example from TI-RTOS to FreeRTOS is to create a
new projectspec file. A projectspec, or project specification file, is used to
create a new project based on predefined settings. For more information on
projectspec files, see the `ProjectSpecs in CCS <https://software-dl.ti.com/ccs/esd/documents/ccs_projectspecs.html>`_
page. In this section, we will be using the ``multi_role`` example as a guide to
convert the ``simple_central`` project to FreeRTOS.

Most embedded applications are built the same way: a main loop that receives
messages from the iCall or from the application itself. This "loop" is
implemented and located inside the ``multi_role`` example so, the developer can
take the example from there. This means that the majority of the application
code can be reused with slight modifications.

In this section, we will be using the ``multi_role`` FreeRTOS example as a guide
to convert the ``simple_central`` project to FreeRTOS. The same can be used to
convert any BLE application into FreeRTOS + GCC.

.. important::

   If you are starting with an example that already enables FreeRTOS (i.e. if
   using ``multi_role`` imported from |SDK|), skip the section below and
   jump to :ref:`sec_freertos_migration_application`.

Modify the Project Properties to support FreeRTOS
^^^^^^^^^^^^^^^^^^^^^^^^^^^^^^^^^^^^^^^^^^^^^^^^^

The goal of this section is to inherit the project configuration settings from
an existing example project that is already setup for FreeRTOS.

#. Setup the new project folders. Create a freertos folder inside the
   ``simple_central`` project directory located in: 
   ``{SDK_INSTALL_DIR}\examples\rtos\CC26X2R1_LAUNCHXL\ble5stack\simple_central``

#. Create a new projectspec file. Copy the gcc folder from ``multi_role/freertos/gcc``
   to ``simple_central/freertos/gcc`` and rename the projectspec from
   ``multi_role_CC26X2R1_LAUNCHXL_freertos_gcc.projectspec`` to 
   ``simple_central_CC26X2R1_LAUNCHXL_freertos_gcc.projectspec``. 
   
#. Ensure the linker file ``CC26X2R1_LAUNCHXL_FREERTOS.lds`` is copied inside
   ``simple_central/freertos/gcc`` if not already done.

#. Update ``simple_central_CC26X2R1_LAUNCHXL_freertos_gcc.projectspec``, find
   and replace all ``multi_role`` with ``simple_central``.

#. By comparing the projectspecs, there will be some files that will need to be
   added or removed. 

    * ``simple_central_CC26X2R1_LAUNCHXL_freertos_gcc.projectspec`` new (FreeRTOS + gcc)
    * ``simple_central_CC26X2R1_LAUNCHXL_tirtos_ccs.projectspec`` legacy (TI-RTOS + CCS)

   The following diff below shows files that are used by ``multi_role`` for its
   peripheral service declarations. Since we are using the ``simple_central``
   example, these are not needed and can be removed.

   .. code-block:: diff
     :caption: Files removed from the new projectspec
    
     -<file path="${COM_TI_SIMPLELINK_CC13XX_CC26XX_SDK_INSTALL_DIR}/source/ti/ble5stack/profiles/dev_info/cc26xx/devinfoservice.c" openOnCreation="false" excludeFromBuild="false" action="link" targetDirectory="Profiles">
     -</file>
     -<file path="${COM_TI_SIMPLELINK_CC13XX_CC26XX_SDK_INSTALL_DIR}/source/ti/ble5stack/profiles/dev_info/devinfoservice.h" openOnCreation="false" excludeFromBuild="false" action="link" targetDirectory="Profiles">
     -</file>
     -<file path="${COM_TI_SIMPLELINK_CC13XX_CC26XX_SDK_INSTALL_DIR}/source/ti/ble5stack/inc/gatt_profile_uuid.h" openOnCreation="false" excludeFromBuild="false" action="link" targetDirectory="Profiles">
     -</file>
     -<file path="${COM_TI_SIMPLELINK_CC13XX_CC26XX_SDK_INSTALL_DIR}/source/ti/ble5stack/host/gatt_uuid.c" openOnCreation="false" excludeFromBuild="false" action="link" targetDirectory="Profiles">
     -</file>
     -<file path="${COM_TI_SIMPLELINK_CC13XX_CC26XX_SDK_INSTALL_DIR}/source/ti/ble5stack/inc/gatt_uuid.h" openOnCreation="false" excludeFromBuild="false" action="link" targetDirectory="Profiles">
     -</file>
     -<file path="${COM_TI_SIMPLELINK_CC13XX_CC26XX_SDK_INSTALL_DIR}/source/ti/ble5stack/host/gattservapp_util.c" openOnCreation="false" excludeFromBuild="false" action="link" targetDirectory="Profiles">
     -</file>
     -<file path="${COM_TI_SIMPLELINK_CC13XX_CC26XX_SDK_INSTALL_DIR}/source/ti/ble5stack/profiles/simple_profile/cc26xx/simple_gatt_profile.c" openOnCreation="false" excludeFromBuild="false" action="link" targetDirectory="Profiles">
     -</file>
     -<file path="${COM_TI_SIMPLELINK_CC13XX_CC26XX_SDK_INSTALL_DIR}/source/ti/ble5stack/profiles/simple_profile/simple_gatt_profile.h" openOnCreation="false" excludeFromBuild="false" action="link" targetDirectory="Profiles">
     -</file>

.. _sec_freertos_migration_application:

Modify the application code to support FreeRTOS
^^^^^^^^^^^^^^^^^^^^^^^^^^^^^^^^^^^^^^^^^^^^^^^

This section describes the changes to the application code that are necessary to
support FreeRTOS. It is recommended to import the ``multi_role``
FreeRTOS project and search for the predefined symbol ``FREERTOS``. This will
reveal the modifications to the ``multi_role`` application that were done. The
following steps are provided using the search mentioned in the previous section
as a guide.

The diffs below provide an overview of all the differences and changes between
the legacy (TI-RTOS + CCS) ``multi_role`` example and the new (FreeRTOS + gcc)
``multi_role`` example. These changes should be applied to the corresponding
``simple_central`` example.

#. Replace all the TI-RTOS calls with DPL/FreeRTOS/POSIX calls in ``simple_central.c``. 

   .. code-block:: diff
      :caption: multi_role FreeRTOS differences - INCLUDES

      +#ifdef FREERTOS
      +#include <FreeRTOS.h>
      +#include <task.h>
      +//#include <pthread.h>
      +#include <mqueue.h>
      +#else
      #include <string.h>
      #include <ti/sysbios/knl/Clock.h>
      #include <ti/sysbios/knl/Event.h>
      #include <ti/sysbios/knl/Queue.h>
      #include <ti/sysbios/knl/Task.h>
      +#endif

      #ifdef FREERTOS
      #include <stdarg.h>
      #endif

      #include <ti/display/Display.h>

      +#if (!(defined FREERTOS) && !(defined __TI_COMPILER_VERSION__)) && !(defined(__clang__))
      #include <intrinsics.h>
      #endif

   .. code-block:: diff
      :caption: multi_role FreeRTOS differences - STACK SIZE

      #ifndef MR_TASK_STACK_SIZE
      +#ifdef FREERTOS
      +#define MR_TASK_STACK_SIZE                   2048
      +#else
      #define MR_TASK_STACK_SIZE                   1024
      +#endif
     
   .. code-block:: diff
      :caption: multi_role FreeRTOS differences - EVENT QUEUE

      /*********************************************************************
      * GLOBAL VARIABLES
      */
      +#ifdef FREERTOS
      +mqd_t g_EventsQueueID;
      +#endif

   .. code-block:: diff
      :caption: multi_role FreeRTOS differences - ICall_Sync

      /*********************************************************************
      * LOCAL VARIABLES
      */

      // Entity ID globally used to check for source and/or destination of messages
      static ICall_EntityID selfEntity;

      // Event globally used to post local events and pend on system and
      // local events.
      +#ifdef FREERTOS
      +ICall_SyncHandle syncEvent;
      +#else
      static ICall_SyncHandle syncEvent;
      +#endif

   .. code-block:: diff
      :caption: multi_role FreeRTOS differences - TASK VARIABLES

      +#ifdef FREERTOS
      +/*Non blocking queue */
      +mqd_t g_POSIX_appMsgQueue;

      +#else
      // Queue object used for app messages
      static Queue_Struct appMsg;
      static Queue_Handle appMsgQueue;
      +#endif

      // Task configuration
      +#ifdef FREERTOS
      +typedef uint32_t * Task_Handle;
      +TaskHandle_t mrTask = NULL;
      +#else
      Task_Struct mrTask;
      +#endif

      +#ifndef FREERTOS
      #if defined __TI_COMPILER_VERSION__
      #pragma DATA_ALIGN(mrTaskStack, 8)
      +#else
      +#pragma data_alignment=8
      +#endif
      +#ifndef FREERTOS
      uint8_t mrTaskStack[MR_TASK_STACK_SIZE];
      +#endif
      +#endif

   .. code-block:: diff
      :caption: multi_role FreeRTOS differences - LOCAL FUNCTIONS

      /*********************************************************************
      * LOCAL FUNCTIONS
      */
      static void multi_role_init(void);
      static void multi_role_scanInit(void);
      static void multi_role_advertInit(void);

      +#ifdef FREERTOS
      +static void multi_role_taskFxn(void *a0);
      +#else//TI_RTOS
      static void multi_role_taskFxn(UArg a0, UArg a1);
      +#endif
      
      //..
      //..
      //..

      +#ifdef FREERTOS
      +static void multi_role_clockHandler(void * arg);
      +#else
      static void multi_role_clockHandler(UArg arg);
      +#endif

   .. code-block:: diff
      :caption: multi_role FreeRTOS differences - multi_role_createTask

      /*********************************************************************
      * @fn      multi_role_createTask
      *
      * @brief   Task creation function for multi_role.
      *
      * @param   None.
      *
      * @return  None.
      */


      void multi_role_createTask(void)
      {

      +#ifdef FREERTOS
      +    BaseType_t xReturned;
      +
      +    /* Create the task, storing the handle. */
      +    xReturned = xTaskCreate(
      +            multi_role_taskFxn,                     /* Function that implements the task. */
      +            "MULTI_ROLE_APP",                       /* Text name for the task. */
      +            MR_TASK_STACK_SIZE / sizeof(uint32_t),  /* Stack size in words, not bytes. */
      +            ( void * ) NULL,                        /* Parameter passed into the task. */
      +            MR_TASK_PRIORITY,                       /* Priority at which the task is created. */
      +            &mrTask );                              /* Used to pass out the created task's handle. */
      +
      +    if(xReturned == errCOULD_NOT_ALLOCATE_REQUIRED_MEMORY)
      +    {
      +        /* Creation of FreeRTOS task failed */
      +        while(1);
      +    }
      +#else
            Task_Params taskParams;

            // Configure task
            Task_Params_init(&taskParams);
            taskParams.stack = mrTaskStack;
            taskParams.stackSize = MR_TASK_STACK_SIZE;
            taskParams.priority = MR_TASK_PRIORITY;
            Task_construct(&mrTask, multi_role_taskFxn, &taskParams, NULL);

      +#endif

      }

   .. code-block:: diff
      :caption: multi_role FreeRTOS differences - multi_role_init()

      +#ifdef FREERTOS
      +  Util_constructQueue(&g_POSIX_appMsgQueue);
      +#else
         // Create an RTOS queue for message from profile to be sent to app.
         appMsgQueue = Util_constructQueue(&appMsg);
      +#endif
         // Create one-shot clock for internal periodic events.
      +#ifdef FREERTOS
      +  Util_constructClock(&clkPeriodic,(void*) multi_role_clockHandler,
      +                        MR_PERIODIC_EVT_PERIOD, 0, false,
      +                        (void*)&periodicUpdateData);
      +#else

         Util_constructClock(&clkPeriodic, multi_role_clockHandler,
                              MR_PERIODIC_EVT_PERIOD, 0, false,
                              (UArg)&periodicUpdateData);
      +#endif

   .. note:: 
      ``simple_central`` does not make use of a periodic timer like the
      one shown above. The above change should be performed to any clock
      constructed in the application using *Util_constructClock(*) to avoid
      build issues.

   .. code-block:: diff
      :caption: multi_role FreeRTOS differences - multi_role_taskFxn

      /*********************************************************************
      * @fn      multi_role_taskFxn
      *
      * @brief   Application task entry point for the multi_role.
      *
      * @param   a0, a1 - not used.
      *
      * @return  None.
      */
      +#ifdef FREERTOS
      +static void multi_role_taskFxn(void* a0)
      +#else
      static void multi_role_taskFxn(UArg a0, UArg a1)
      +#endif
      {
         // Initialize application
         multi_role_init();

         // Application main loop
         for (;;)
         {
            uint32_t events;

            // Waits for an event to be posted associated with the calling thread.
            // Note that an event associated with a thread is posted when a
            // message is queued to the message receive queue of the thread

      +#ifdef FREERTOS
      +    mq_receive(syncEvent, (char*)&events, sizeof(uint32_t), NULL);
      +#else
            events = Event_pend(syncEvent, Event_Id_NONE, MR_ALL_EVENTS,
                              ICALL_TIMEOUT_FOREVER); // event_31 + event_30
      +#endif

            if (events)

      //..
      //..
      //..

               // If RTOS queue is not empty, process app message.
            if (events & MR_QUEUE_EVT)
            {
      +#ifdef FREERTOS
      +
      +         mrEvt_t *pMsg;
      +         do {
      +             pMsg = (mrEvt_t *)Util_dequeueMsg(g_POSIX_appMsgQueue);
      +             if (NULL != pMsg)
      +             {
      +                 // Process message.
      +                 multi_role_processAppMsg(pMsg);
      +
      +                // Free the space from the message.
      +                ICall_free(pMsg);
      +             }
      +             else
      +             {
      +                 break;
      +             }
      +           }while(1);
      +#else
                  while (!Queue_empty(appMsgQueue))
                     {
                        mrEvt_t *pMsg = (mrEvt_t *)Util_dequeueMsg(appMsgQueue);
                        if (pMsg)
                        {
                        // Process message.
                        multi_role_processAppMsg(pMsg);

                        // Free the space from the message.
                        ICall_free(pMsg);
                        }
                     }
      +#endif
            }

   .. code-block:: diff
      :caption: multi_role FreeRTOS differences - multi_role_advertInit

         if (addrMode > ADDRMODE_RANDOM)
         {
            multi_role_updateRPA();
      +#ifdef FREERTOS
      +    // Create one-shot clock for RPA check event.
      +    Util_constructClock(&clkRpaRead, (void*)multi_role_clockHandler,
      +                        READ_RPA_PERIOD, 0, true,
      +                        (void*) &argRpaRead);
      +
      +#else
            // Create one-shot clock for RPA check event.
            Util_constructClock(&clkRpaRead, multi_role_clockHandler,
                              READ_RPA_PERIOD, 0, true,
                              (UArg) &argRpaRead);
      +#endif
         }
      }

   .. code-block:: diff
      :caption: multi_role FreeRTOS differences - multi_role_enqueueMsg

            pMsg->pData = pData;

            // Enqueue the message.
      +#ifdef FREERTOS
      +    success = Util_enqueueMsg(g_POSIX_appMsgQueue, syncEvent, (uint8_t *)pMsg);
      +#else
            success = Util_enqueueMsg(appMsgQueue, syncEvent, (uint8_t *)pMsg);
      +#endif
            return (success) ? SUCCESS : FAILURE;
         }

   .. code-block:: diff
      :caption: multi_role FreeRTOS differences - multi_role_clockHandler

      /*********************************************************************
      * @fn      multi_role_clockHandler
      *
      * @brief   Handler function for clock timeouts.
      *
      * @param   arg - event type
      *
      * @return  None.
      */
      +#ifdef FREERTOS
      +static void multi_role_clockHandler(void * arg)
      +#else
      static void multi_role_clockHandler(UArg arg)
      +#endif
      {

   .. code-block:: diff
      :caption: multi_role FreeRTOS differences - multi_role_handleKeys

      /*********************************************************************
      * @fn      multi_role_handleKeys
      *
      * @brief   Handles all key events for this device.
      *
      * @param   keys - bit field for key events. Valid entries:
      *                 HAL_KEY_SW_2
      *                 HAL_KEY_SW_1
      *
      * @return  none
      */
      static void multi_role_handleKeys(uint8_t keys)
      {
      +#ifndef FREERTOS
            uint32_t rtnVal = 0;
      +#endif
            if (keys & KEY_LEFT)
         {
      +#ifndef FREERTOS
            // Check if the key is still pressed
            if (PIN_getInputValue(CONFIG_GPIO_BTN1) == 0)
            {
      +#endif
            tbm_buttonLeft();
      +#ifndef FREERTOS
            }
      +#endif
         }
         else if (keys & KEY_RIGHT)
         {
            // Check if the key is still pressed
      +#ifndef FREERTOS
            rtnVal = PIN_getInputValue(CONFIG_GPIO_BTN2);
            if (rtnVal == 0)
            {
      +#endif
            tbm_buttonRight();
      +#ifndef FREERTOS
            }
      +#endif
         }
      } 

   .. code-block:: diff
      :caption: multi_role FreeRTOS differences - multi_role_addConnInfo

                  // Create a clock object and start
                  connList[i].pUpdateClock
                  = (Clock_Struct*) ICall_malloc(sizeof(Clock_Struct));

                  if (connList[i].pUpdateClock)
                  {
      +#ifdef FREERTOS
      +              Util_constructClock(connList[i].pUpdateClock,
      +                                              (void*)multi_role_clockHandler,
      +                                              SEND_PARAM_UPDATE_DELAY, 0, true,
      +                                              (void*) connList[i].pParamUpdateEventData);
      +
      +#else
                     Util_constructClock(connList[i].pUpdateClock,
                                          multi_role_clockHandler,
                                       SEND_PARAM_UPDATE_DELAY, 0, true,
                                       (UArg) connList[i].pParamUpdateEventData);
      +#endif
                  }
                  else
                  {

   .. note:: 
      There are other clocks (i.e. pRssiClock) defined in the
      ``simple_central`` project. Make sure to apply the above change to those
      instances as shown in the code snippet below, take note of the new
      *scClockEventData_t* structure used to pass in arguments. This can be
      taken from ``multi_role.c`` file and renamed.

      The example below shows the syntax required when passing in parameters to
      the Util_constructClock() function using FreeRTOS. Simply put, logical
      statements made inside the function call will result in a build issue.

   .. code-block:: diff
      :caption: simple_central::SimpleCentral_StartRssi() - Clock construction

            if (connList[connIndex].pRssiClock)
         {
      +#ifdef FREERTOS
      +    scClockEventData_t locData;
      +    locData.event = (connIndex << 8) | SC_EVT_READ_RSSI;
      +
      +    // Create one-shot clock for RPA check event.
      +    Util_constructClock(connList[connIndex].pRssiClock,
      +                        (void*)SimpleCentral_clockHandler,
      +                        DEFAULT_RSSI_PERIOD, 0, true,
      +                        (void*)&locData);
      +#else      
            Util_constructClock(connList[connIndex].pRssiClock,
                              SimpleCentral_clockHandler,
                              DEFAULT_RSSI_PERIOD, 0, true,
                              (connIndex << 8) | SC_EVT_READ_RSSI);
      +#endif                        
         }

   While searching for the macro **FREERTOS** in the project, you will find
   changes to other files (i.e. ``util.c/h``, ``icall_user_config.c``, etc).
   These changes do not need to be applied to the new example because these
   files are inherited directly from the SDK.

#. Modify main_freertos.c

   .. code-block:: diff
     :caption: Modifying main.c - include
 
     #include "bcomdef.h"
     -#include "multi_role.h"
     +#include "simple_central.h"

   .. code-block:: diff
     :caption: Modifying main.c - createTask
 
     /* Kick off application - Priority 1 */
     -multi_role_createTask();
     +SimpleCentral_createTask();

#. Modify the .syscfg file using a text editor to change the target rtos to 
   freertos.

   .. code-block:: diff
      :caption: multi_role freertos differences - SysConfig

      */
      -// @cliArgs --board /ti/boards/CC26X2R1_LAUNCHXL --rtos tirtos
      +// @cliArgs --board /ti/boards/CC26X2R1_LAUNCHXL --rtos freertos

      /*
      *  simple_central.syscfg
      */

.. caution:: 
   **Workaround for Button Debouncing**

   There exists a known issue with FreeRTOS projects in the |BLE5_STACK| (see
   Release Notes for more information). This issue affects only the usage of the
   example application's two button menu. To workaround this, manually add a
   delay inside board_key.c::Board_keyCallback, as opposed to starting a
   FreeRTOS timer. Below is an example of the modification:

   .. code-block:: diff
      :caption: Reworking the Pin debounce timer

      //define this outside the function
      +#define CPU_convertMsToDelayCycles(milliseconds) \
      +   (((uint32_t)(milliseconds)) * (48000 / 3))
      
      //Place the below changes at the end of Board_keyCallback
               keysPressed |= KEY_RIGHT;
      }
      #endif

      +#ifdef FREERTOS
      +/* 100 ms delay */
      +CPUdelay(CPU_convertMsToDelayCycles(100));

      +// Notify the application
      +(*appKeyChangeHandler)(keysPressed);
      +#else
      Util_startClock(&keyChangeClock);
      +#endif