Segger J-Link support for CC1312PSIP in |IAR|
^^^^^^^^^^^^^^^^^^^^^^^^^^^^^^^^^^^^^^^^^^^^^

To be able to use a Segger J-Link probe with the CC1312PSIP in |IAR|, some
configuration is required. Please configure the following in your |IAR|
project settings.

1. .. |iar_segger_jlink_settings_1| image:: /debugging/resources/iar_segger_jlink_settings_1.png
2. .. |iar_segger_jlink_settings_2| image:: /debugging/resources/iar_segger_jlink_settings_2.png
3. .. |iar_segger_jlink_settings_3| image:: /debugging/resources/iar_segger_jlink_settings_3.png

.. note:: if |IAR| complains about the wrong CPU type, we need to modify the .ewp file which is located 
    in the workspace of IAR as follows:

.. |iar_segger_jlink_cputype| image:: /debugging/resources/iar_segger_jlink_cputype.png