Segger J-Link support for CC1312PSIP in |CCS|
^^^^^^^^^^^^^^^^^^^^^^^^^^^^^^^^^^^^^^^^^^^^^

To be able to use a Segger J-Link probe with the CC1312PSIP in |CCS|, some
configuration is required. Please configure the following in your |CCS|
project settings, under **General**.

.. |ccs_segger_jlink_settings_1| image:: /debugging/resources/ccs_segger_jlink_settings_1.png

When launching a debugging session, J-Link will state that the CC1312PSIP is
not supported. 

.. |ccs_segger_jlink_settings_1| image:: /debugging/resources/ccs_segger_jlink_settings_2.png

You can fix that by clicking OK, and instead picking the CC1312R1, as follows:

.. |ccs_segger_jlink_settings_1| image:: /debugging/resources/ccs_segger_jlink_settings_3.png