Using the Memory Browser
========================

.. XXX this is only for CCS

Debuggers are able to show a representation of the memory on the |DEVICE|.  In
:term:`CCS`, you can index by address or by symbol name. As an example, consider the stack 
that was overrun in :numref:`fig-rov-task-detailed`:

===============================================================  =================================================================
Simple Peripheral Task's stack. Note ``BE`` watermark            GAPRole Task's stack. Note it's completely filled.
---------------------------------------------------------------  -----------------------------------------------------------------
.. figure:: /debugging/resources/mem_browser_sbp_stack.png        .. figure:: /debugging/resources/mem_browser_gaprole_stack.png
===============================================================  =================================================================

CCS Theia also includes a memory browser, click on ``view`` into 
``memory`` to enter memory browser. 

.. figure:: /debugging/resources/ccs_theia_memory_browser.png
    :align: center

    CCS Theia memory browser 

The solution in this case would be to increase the stack size for the failing
task and see what the stack peak really is. The ``stackPeak`` reported is
relying on how many watermark bytes are overwritten, so it can't know how much
the overrun amounts to.

Because stacks are utilized from higher addresses towards lower addressed
(upwards in the picture), stacks that overrun will tend to overwrite data at
locations immediately before the stack.