.. |img_icon_debug_iar| image:: /debugging/resources/icon_debug_iar.png

Connecting to the XDS Debugger
^^^^^^^^^^^^^^^^^^^^^^^^^^^^^^

If only one debugger is attached, the IDE uses it automatically when you click
the |img_icon_debug_ccs| button in CCS

.. Commenting out while IAR IDE is not available for CC23xx
  or |img_icon_debug_iar| in IAR.


If **multiple debuggers** are connected, you must choose the individual
debugger to use. The following steps detail how to select a debugger in CCS

.. Commenting out while IAR IDE is not available for CC23xx
  and IAR.

.. Commenting out while IAR IDE is not available for CC23xx
  Configuring Debugger in IAR
  ---------------------------
  
  If only one debugger is attached, IAR uses it automatically when you click the
  |img_icon_debug_iar| button.
  
  
  If more than one debug probe is connected, use the following steps to have IAR
  always prompt to select the connection.
  
  1. Open the project options (\ ``Project`` |rarr| ``Options``)
  
  2. Go to the Debugger entry.
  
  3. Go to Extra options.
  
  4. Add the following command line option: ``--drv_communication=USB:#select``