Deciphering CPU Exceptions
==========================

Several possible exception causes exist. If an exception is caught, an
exception handler function can be called. Depending on the project settings,
this handler may be a default handler in ROM, which is just an infinite loop or
a custom function called from this default handler instead of a loop.

When an exception occurs, the exception may be caught and halted in debug mode
immediately, depending on the debugger. If the execution halted manually later
through the Break debugger, it is then stopped within the exception handler
loop.

Exception Cause
---------------

With the default setup using TI-RTOS, the exception cause can be found in the
System Control Space register group (``CPU_SCS``) in the register ``CFSR``
(Configurable Fault Status Register). The `Arm Cortex User Guide`_ describes
this register. Most exception causes fall into the following three categories.

* Stack overflow or corruption leads to arbitrary code execution.

  * Almost any exception is possible.

* A NULL pointer has been dereferenced and written to.

  * Typically (IM)PRECISERR exceptions

* A peripheral module (like UART, Timer, and so forth) is accessed
  without being powered.

  * Typically (IM)PRECISERR exceptions

The ``CFSR`` register is available in ``View`` |rarr| ``Registers``.

When an access violation occurs, the exception type is IMPRECISERR because
writes to flash and peripheral memory regions are mostly buffered writes.

If the ``CFSR:BFARVALID`` flag is set when the exception occurs (typical for
PRECISERR), the ``BFAR`` register in ``CPU_SCS`` can be read out to find which
memory address caused the exception.

If the exception is IMPRECISERR, PRECISERR can be forced by manually disabling
buffered writes. Set ``CPU_SCS:ACTRL:DISDEFWBUF`` to 1, by either manually
setting the bit in the register view in the debugger or by including
``<hw_cpu_scs.h>`` from Driverlib and calling the following.

.. code-block:: c

    #include <ti/devices/cc26x0r2/inc/hw_cpu_scs.h>
    //..
    int main()
    {
        // Disable write-buffering. Note that this negatively affect performance.
        HWREG(CPU_SCS_BASE + CPU_SCS_O_ACTLR) = CPU_SCS_ACTLR_DISDEFWBUF;
        // ..
    }

Using TI-RTOS and ROV to Parse Exceptions
-----------------------------------------

To enable exception decoding in the RTOS Object View (ROV) without using too
much memory, use the Minimal exception handler in TI-RTOS. The default choice
in the |STACK| projects is to use no exception handler.

.. ifconfig:: device in ['cc13x0', 'cc2640']

    To set this up, change the section of the TI-RTOS configuration file that
    relates to M3Hwi so that it looks like the code below:

    .. code-block:: js

        //m3Hwi.enableException = true;
        m3Hwi.enableException = false;
        //m3Hwi.excHandlerFunc = null;
        m3Hwi.excHookFunc = "&execHandlerHook";

    Then, make a function somewhere with the signature ``void
    (*Hwi_ExceptionHookFuncPtr)(Hwi_ExcContext*);`` such as the one below:

    .. code-block:: c

        #include <ti/sysbios/family/arm/m3/Hwi.h>
        // ...
        volatile uintptr_t *excPC = 0;
        volatile uintptr_t *excCaller = 0;
        // ...
        void execHandlerHook(Hwi_ExcContext *ctx)
        {
            excPC = ctx->pc;     // Program counter where exception occurred
            excCaller = ctx->lr; // Link Register when exception occurred

            while(2);
        }



    Setting ``m3Hwi.enableException`` to false enables the minimal handler,
    which fills out the global ``Hwi_ExcContext`` structure that the ROV looks
    at to show the decoded exception. By setting up an excHookFunc, the minimal
    exception handler will call this function and pass along a pointer to the
    exception context for the user to work with. This structure is defined in
    ``<ti/sysbios/family/arm/m3/Hwi.h>``.

.. ifconfig:: device == 'cc13xx_cc26xx'

    To set this up, open the project's SysConfig file (.syscfg) and navigate to
    ``TI-RTOS`` |rarr| ``HAL`` |rarr| ``Hwi`` and select the
    ``Enable Exception Decoding at runtime`` option.

    SysConfig sets the default exception handler to ``Hwi_excHandlerMax``, which
    uses the Error module to pass up errors to a customized function. To
    customize this, navigate to ``TI-RTOS`` |rarr| ``RUNTIME`` |rarr|
    ``Error Handling`` and enter in an
    ``Optional function to call when an error is raised``.

When an exception occurs, the device should end up in that infinite loop.
Inspect the ``ROV`` |rarr| ``Hwi`` |rarr| ``Exception information``.

.. figure:: /debugging/resources/rov_hwi_exception.png
    :align: center

    Decoded exception, intentional write to address 0x0013 which is illegal.
    Note that writebuffering has been disabled to get a precise error location,
    and that m3Hwi.enableException has been set to false to get the decoding.

In this case, a bus fault was forced in the function writeToAddress by
dereferencing address 0x0013 and trying to write to it:

.. code-block:: c
    :caption: Write to an address in the FLASH memory region.

    void writeToAddress(uintptr_t *addr, int val)
    {
        *(int *)addr = val;
    }

    // ..

    void taskFxn(...)
    {
        // ..
        writeToAddress( (void*)19, 4 ); // Randomly chosen values
    }

The write instruction was placed on line 79 of ``application.c``, as indicated.  To
get a precise location, the write buffer was disabled as described earlier.

It can be instructive to look at the disassembly view for the locations
specified by PC (program counter) and LR (link register). PC is the presumed
exception location, and LR is normally the location the failing function should
have returned to. As an example, the PC at this exception:

.. figure:: /debugging/resources/exception_pc_of_write.png
    :align: center

    Here the ``pc`` from the decoded exception was looked up in the disassembly
    view.

Some forensics is required here. We have from the Hwi decoding in ROV (and from
the exception context in the exception hook) that the program counter was
``0x708e`` when the exception occurred.

At that location there is a store instruction ``str r0, [r1]`` meaning, store
in R0 the value of what the memory address in R1 points to. The business with
``SP`` in the figure above is related to optimization being turned off, so all
local variables are stored on the stack, even though in this case R0 and R1
could have been used directly from the caller.

Now we know that the exception occurred because someone called
``writeToAddress`` with an invalid address.

Thanks to the exception decoder we can easily find the call site by looking at
the call stack, but if the call stack isn't helpful, we can look at ``lr``,
which is seen in the exception decoder to be ``0x198f``

.. figure:: /debugging/resources/exception_lr_of_write.png
    :align: center

    Call site as specified in ``lr``. Note that lr is the instruction after the
    call to ``writeToAddress`` because execution would have resumed here.

We can see here that R0 and R1 are initialized with constants. This means that
some programmer has intentionally called the write function with an address
that causes a busfault.

Most often the reason for a bus-fault is that a pointer is not initialized and
a function like ``writeToAddress`` gets the pointer, assumes it's valid and
dereferences the pointer and writes to the invalid address.