Breakpoints in IAR
------------------

.. note::
    IAR reserves one comparator for instruction stepping.

To toggle a breakpoint, do any of the following.

-  Single-click the area to the left of the line number.

-  Go to the line and press ``F9`` to toggle breakpoint

-  Right-click on the line and select Toggle Breakpoint (Code).

A breakpoint looks like this:

.. figure:: /debugging/resources/iar_breakpoint_ex.png
    :align: center

    Breakpoint on ``PIN_init()``. Debugger halted at start of main().


For an overview of the active and inactive breakpoints, click
``View`` |rarr| ``Breakpoints``.

.. figure:: /debugging/resources/iar_breakpoint_list.png
    :align: center

    List of breakpoints. Right-click to edit options, or de-select to deactivate.

To set a conditional break, do as follows.

1. Right-click the breakpoint in the overview.

2. Choose Edit....

When debugging, Skip Count and Condition can help skip a number of
breaks or only break if a variable is a certain value.

.. note::
    Conditional breaks require a debugger response and may halt the processor
    long enough to break an active RF connection, or otherwise disrupt timing
    on the debug target.