.. _sec-coexistence:

Coexistence
===========

The coexistence (coex) feature is a means to organize wireless packet traffic for
communication protocols operating in the same frequency band. Instead of interfering
with each other's transmissions, affecting the RF performance, two co-located devices
will have a dedicated communication interface to signal and determine access to the
shared frequency band.

The coex feature is not a standard, but is rooted in the recommendations provided by
|COEXSTD|: "Coexistence of Wireless Personal Area Networks with Other Unlicensed
Frequency Bands Operating Wireless Devices". The industry approach is more of a
"best-practice" when it comes to this feature, and every device supporting a
coexistence interface is free to implement its own solution to the problem.

The coex interface implemented for |DEVICE| is compatible with
Wi-Fi devices that support Packet Traffic Arbitration (:term:`PTA`). This is one of the
approaches recommended and described by |COEXSTD|. This approach is based on a shared
PTA control module between the coexisting devices, to decide which device is permitted
to communicate in the shared frequency band. Many Wi-Fi devices implement their version
of such a module, and the implemented coex feature is based on the assumption that the
PTA control module is embedded in the Wi-Fi device. The Wi-Fi device will therefore
have a master role in this coex device scheme, as it controls the PTA logic. The
coexistence interface can be abstracted to a signal interface between the two devices,
as illustrated in the figure below. For an example of supported Wi-Fi devices, see  
|CC3235SF|, and see |COEXAPPNOTE| application note for an example of coexistence
solutions.

.. figure:: /coexistence/resources/block-diagram_coex-interface-abstraction.png
    :align: center
    :width: 70%

    Block-diagram of coexistence interface abstraction


.. _sec-pta-interface:

Packet Traffic Arbitration (PTA) Interface
------------------------------------------

The :term:`PTA` interface between the two devices is a set of wired signals. What
information to communicate, and ultimately the number of signals used, will depend on
the implementation of the PTA control module. Based on the most common Wi-Fi PTA
implementations, the implemented coex feature supports three sets of signals.
These sets of signals, or *coex modes*, are named:

* 3-Wire
* 1-Wire REQUEST
* 1-Wire GRANT

From the naming scheme, it is obvious that the supported coex modes use at max three
wires to signal state information to the Wi-Fi device. However, the two 1-Wire modes
can be seen as subsets of the signaling provided by 3-Wire mode. As illustrated in the
table below, the 3-Wire mode utilizes all the provided signals, and for both 1-Wire
REQUEST and 1-Wire GRANT two of the signals are disabled.

.. table:: Mapping of coex mode and PTA signals.

    +----------------+----------+----------+----------+
    |                | PTA Coex Signals               |
    +----------------+----------+----------+----------+
    | Coex Mode      | REQUEST  | PRIORITY | GRANT    |
    +================+==========+==========+==========+
    | 3-Wire         |    X     |    X     |    X     |
    +----------------+----------+----------+----------+
    | 1-Wire REQUEST |    X     |          |          |
    +----------------+----------+----------+----------+
    | 1-Wire GRANT   |          |          |    X     |
    +----------------+----------+----------+----------+

Furthermore, the supported coex modes can be illustrated as in the block-diagrams
in the figures below. Seen from the BLE device, the REQUEST and PRIORITY signals are
defined as outputs, and the GRANT signal is defined as an input.

.. ifconfig:: device == 'cc13xx_cc26xx'

    .. figure:: /coexistence/resources/block-diagram_coex-3-wire.png
        :align: center
        :width: 70%

        Block-diagram of coexistence mode **3-Wire**

    .. figure:: /coexistence/resources/block-diagram_coex-1-wire-REQUEST.png
        :align: center
        :width: 70%

        Block-diagram of coexistence mode **1-Wire REQUEST**

    .. figure:: /coexistence/resources/block-diagram_coex-1-wire-GRANT.png
        :align: center
        :width: 70%

        Block-diagram of coexistence mode **1-Wire GRANT**

.. ifconfig:: device == 'cc23xx'

    .. attention::
        MAKE NEW PLOTS HERE!!!!!

All coexistence modes are not supported on all Wi-Fi devices. The SimpleLink
CC3135 and CC3235 Wi-Fi devices only support the 1-Wire REQUEST mode. 

.. _sec-coex-signaling:

Coexistence Signaling
---------------------

The coexistence signaling approach for the 3-Wire mode, using the three available
signals, can be summarized in two steps:

1. Coex slave (BLE device) requests permission to perform RF activity, with info on:

   * Priority of the request (low/high)

   * Type of RF activity (TX/RX)

2. Coex master (Wi-Fi device) will grant or deny the request

From the coex slave perspective, the above two steps are implemented by configuration
of the following signals for the PTA interface:

* Coex **REQUEST** signal:

    This is an output signal, controlled by the coex slave. This signal is used to
    indicate a request to use the shared frequency band, that is, perform any RF
    activity.

* Coex **PRIORITY** signal:

    This is an output signal, controlled by the coex slave. This signal is
    *time-shared* between first indicating the priority of the access request,
    followed by indicating the type of RF activity (TX/RX) the device will perform. At
    first, when the REQUEST signal is asserted, the value of the PRIORITY signal will
    indicate the *priority* (low/high) of the request. After a defined 20 µs, the
    PRIORITY signal is used to indicate the *type* of RF activity. This means that the
    signal will be de-asserted or asserted depending on if the scheduled activity is
    RX or TX.

* Coex **GRANT** signal:

    This is an input signal, controlled by the coex master. This signal indicates the
    response of the :term:`PTA` decision, that is, whether the request is granted or
    not.

.. note::
    The terms signal **assert** and signal **de-assert** are used to describe the value
    change of a signal to respectively *active* and *idle*. For an *active high*
    signal, the signal is asserted by changing the signal value from low to high. For
    an *active low* signal, the signal is asserted by changing the signal value from
    high to low. For the opposite signal operation, de-assert, the signal value changes
    from active to idle.

    .. table:: Assert and de-assert meaning for signal active/idle level

        +--------------+------------+-----------------+-----------------+
        | Active Level | Idle Level | Assert          | De-assert       |
        +==============+============+=================+=================+
        | **High**     | Low        | Low |rarr| High | High |rarr| Low |
        +--------------+------------+-----------------+-----------------+
        | **Low**      | High       | High |rarr| Low | Low |rarr| High |
        +--------------+------------+-----------------+-----------------+

In order to support time-shared signals, the coex feature is heavily dependent on
accurate *timing*. What makes this implementation compatible with a Wi-Fi device that
supports a PTA interface, is the adherence to such timing requirements. The figure
below illustrates a timing diagram for a BLE device signaling the scheduled RF
activities, receive and transmit respectively. Note that the diagram depicts REQUEST
and PRIORITY signals as active high, but the GRANT signal is by default defined as
*active low*. This means that a coex request is granted when the GRANT signal is driven
low by the Wi-Fi device.

.. _fig-time-diagram:
.. figure:: /coexistence/resources/time-diagram_3-wire.png
    :align: center
    :width: 100%

    Coex 3-Wire timing diagram

The sections marked with red in the diagram, T1 - T5, are intended to highlight the
following signaling and timing requirements to be aware of:

* **T1**: The REQUEST signal is asserted by the coex slave, and indicates to the coex
  master that the coex slave will perform RF activity. This is a request for access to
  the shared frequency band. In the timing diagram, this happens at a time T1 before
  the BLE RX command is scheduled to run. T1 can be expected to be in the range of
  90-150 µs. 

* **T2**: The PRIORITY signal is *time-shared* between indicating *priority* and
  and *type of RF activity* (TX/RX) the BLE device will do. The time T2 indicates the
  duration of which the PRIORITY signal indicates priority; from the time the REQUEST
  signal is asserted, and for a duration of 20 µs. For the rest of the request
  interaction, as long as the REQUEST signal is asserted, the PRIORITY signal
  indicates TX/RX activity.

* **T3**: In a period before the scheduled RF activity, the coex master will assert or
  de-assert the GRANT signal. This is to indicate if the request from the coex slave,
  asserted at **T1**, is granted or not. At period T3, 50-135 µs, the GRANT signal is
  expected to be in a stable state. The coex slave will read the GRANT signal within
  the T3 period, and use this value as the answer to the request.

* **T4**: The PRIORITY signal is *time-shared*, as explained under **T2**. After T2,
  the PRIORITY signal indicates the type of RF activity (and no longer priority). In
  the timing diagram, the coex slave asserts the PRIORITY signal at T4 before it
  transmits, to indicate the change in type of activity; from RX to TX. The RX
  activity is indicated by de-asserting the PRIORITY signal, and the TX activity is
  indicated by asserting the PRIORITY signal. 

* **T5**: After the coex slave is finished with the scheduled RF activities, it will
  de-assert the REQUEST signal. This is how the coex slave indicates to the coex master
  that the requested RF activity is finished. This will happen 0-25 µs after the last
  RF activity.


.. _sec-coex-config:

Configuration Options
---------------------

The coex configuration options are made available from the RF driver module in
SysConfig.

.. figure:: /coexistence/resources/syscfg_coex-config.png
    :align: center
    :width: 80%

    Coexistence configuration options in SysConfig

Depending on the application, use case, and what Wi-Fi device the |DEVICE| 
is intended to coexist with, certain options are up to the
user to configure.  

**Coex mode**: As described in :ref:`sec-pta-interface`, the coex feature can be
configured to interface with PTA controllers based on 3-Wire, 1-Wire REQUEST or 1-Wire
GRANT, which are different combinations of enabling or disabling the supported coex
signals.

**Coex signal idle level**: The signal idle level can be configured as *low* or
*high*, which in other terms means that the same signal is either respectively
*active high* or *active low*. To configure the active levels used in
:ref:`fig-time-diagram`, both REQUEST and PRIORITY are set to idle level low, and
GRANT is set to idle level high. 

**Priority indication time**: As described in :ref:`sec-coex-signaling`, the PRIORITY
signal is time-shared between indicating priority and the type of RF activity. The
Priority Indication Time field in SysConfig specifies how long, in microseconds, the
PRIORITY signal indicates priority before it switches to indicate the type of RF
activity. 

**BLE Use Case Configuration**: Separate configuration can be set for different BLE
use cases (connection establishment, connected, broadcaster, observer) if the
application requires the behavior to differ between these. The following
configuration options can be set for each of these use cases separately:

* **Default priority**: This is the default behavior of the PRIORITY signal when it
  indicates the priority of the coex request. It can be set to either low or high.

* **Assert REQUEST signal for RX**: This option is by default enabled. However,
  depending on the use case and application, the coex behavior can be configured to
  not assert REQUEST for any scheduled RX activities. In this case, the BLE device does
  not care if the Wi-Fi device is performing any RF activities of its own. With
  reference to :ref:`fig-time-diagram`, disabling this option would shift the assertion
  of the REQUEST signal to the right. The REQUEST signal will then be asserted at a
  time T1 before the TX activity instead of the RX activity. This means that both
  REQUEST and PRIORITY signals will stay idle for the RX activity.

**Coex pin mapping**: Depending on the mode, the coex signal(s) used for the PTA
interface with the Wi-Fi device can be mapped to any available DIO pins. This is
configured in the pin mux section of the RF module, as illustrated in the figure
below.

.. figure:: /coexistence/resources/syscfg_coex-pin-selection.png
    :align: center
    :width: 80%

    Coexistence pin mapping