.. _sec-ieee-coexistence:

Wi-Fi Coexistence
=================

The coexistence (coex) feature is a means to organize wireless packet traffic for
communication protocols operating in the same frequency band. Instead of interfering
with each other's transmissions, affecting the RF performance, two co-located devices
will have a dedicated communication interface to signal and determine access to the
shared frequency band.

IEEE 802.15.4-based stacks and Wi-Fi channels both exist in the 2.4 GHz band over the 
same frequency space. When deploying both protocols in the same environments, careful 
planning must be performed to make sure that they don't interfere with each other. 
Coexistence is particularly required when placing the Wi-Fi and 802.15.4 devices on 
the same platform (for example, a combined gateway). In these cases, the isolation 
between the antennas of the two devices is not enough to avoid impact on the 
performance. Without a proper coexistence mechanism, the RX of the 802.15.4 device 
will be affected by the Wi-Fi TX and vice versa. The coexistence mechanism protects the 
RX using GPIOs interface between the devices and allows visibility of the Wi-Fi TX/RX 
activity along with the ability to hold a Wi-Fi transmission.

The coex interface implemented for SimpleLink CC13xx/CC26xx devices is compatible with
Wi-Fi devices that support two-wire coexistence mode.  This approach is based on a shared
control module between the coexisting devices, to decide which device is permitted
to communicate in the shared frequency band. Many Wi-Fi devices implement their version
of such a module, and the implemented coex feature is based on the assumption that the
two-wire control module is embedded in the Wi-Fi device. The Wi-Fi device will therefore
have a host role in this coex device scheme, as it controls the two-wire logic. The
coexistence interface can be abstracted to a signal interface between the two devices,
as illustrated in the figure below. For an example of supported Wi-Fi devices, view the
available `WiLink Products <https://www.ti.com/wireless-connectivity/wi-fi/products.html#p2792=External%20MPU>`_ 

.. figure:: /coexistence/resources/block-diagram_coex-ieee-interface-abstraction.png
    :align: center
    :width: 70%

    Block-diagram of coexistence interface abstraction

    .. note::
        Z-Stack also supports three-wire PTA coexistence, refer to the |COEXISTENCE|
        module for more information on this mode of operation

.. _sec-two-wire-interface:

Two-wire Coex Interface
-----------------------

The supported IEEE 802.15.4 two-wire coex mode can be illustrated as in the 
block-diagram below. Seen from the 802.15.4 device, the REQUEST signal is
defined as an output while the GRANT signal is defined as an input.

.. figure:: /coexistence/resources/block-diagram_coex-2-wire.png
    :align: center
    :width: 70%

    Block-diagram of coexistence mode **2-Wire**

Two-wire coexistence modes are not supported on all Wi-Fi devices. For example,
the SimpleLink CC3135 and CC3235 Wi-Fi devices only support the 1-Wire REQUEST mode. 

.. _sec-two-wire-coex-signaling:

Coexistence Signaling
---------------------

The coexistence signaling approach for the 2-Wire mode, using the two available
signals, can be summarized as follows:

* Coex **REQUEST** signal:

    This is an output signal, controlled by the coex target. This signal is used to
    request that the Wi-Fi device disables transmissions for a given time.  This is
    used during high priority situations for which IEEE 802.15.4 communication
    must proceed in order to maintain the network.  It connects to the PA_SD pin
    of the WiLink device.

* Coex **GRANT** signal:

    This is an input signal, controlled by the coex host. This signal indicates
    whether Wi-Fi transmissions are active so that the 802.15.4 device will not
    execute simultaneous transmissions.  This connects to the WiLink RX line.

.. note::
    The terms signal **assert** and signal **de-assert** are used to describe the value
    change of a signal to respectively *active* and *idle*. For an *active high*
    signal, the signal is asserted by changing the signal value from low to high. For
    an *active low* signal, the signal is asserted by changing the signal value from
    high to low. For the opposite signal operation, de-assert, the signal value changes
    from active to idle.

    .. table:: Assert and de-assert meaning for signal active/idle level

        +--------------+------------+-----------------+-----------------+
        | Active Level | Idle Level | Assert          | De-assert       |
        +==============+============+=================+=================+
        | **High**     | Low        | Low |rarr| High | High |rarr| Low |
        +--------------+------------+-----------------+-----------------+
        | **Low**      | High       | High |rarr| Low | Low |rarr| High |
        +--------------+------------+-----------------+-----------------+

In order to support time-shared signals, the coex feature is heavily dependent on
accurate *timing*. What makes this implementation compatible with a Wi-Fi device that
supports a two-wire interface, is the adherence to such timing requirements.

.. _sec-two-wire-coex-config:

Configuration Options
---------------------

The coex configuration options are made available from the RF driver module in
SysConfig (*TI Drivers* |rarr| *RF*).

.. figure:: /coexistence/resources/syscfg_ieee-coex-config.png
    :align: center
    :width: 80%

    Coexistence configuration options in SysConfig

Depending on the application, use case, and what Wi-Fi device the SimpleLink
CC13xx/CC26xx IEEE 802.15.4 device is intended to coexist with, certain options 
are up to the user to configure.  

**Coex mode**: Only two-wire mode is currently supported for the IEEE 802.15.4 PHY

**Coex signal idle level**: The signal idle level can be configured as *low* or
*high*, which in other terms means that the same signal is either respectively
*active high* or *active low*. By default both REQUEST and GRANT are set to idle
level low.

**Coex pin mapping**: The coex signal(s) used for the two-wire interface with the 
Wi-Fi device can be mapped to any available DIO pins. This is configured in the pin 
mux section of the RF module, as illustrated in the figure below.

.. figure:: /coexistence/resources/syscfg_ieee-coex-pin-selection.png
    :align: center
    :width: 80%

    Coexistence pin mapping

**Coex pin configuration while not in use**: Options are given in regards to the pin
configuration for coexistence REQUEST & GRANT pins while they are not being used.
For the lowest power operation it is recommended that the following selections
be made accordingly.

.. figure:: /coexistence/resources/syscfg_ieee-coex-pin-configuration.png
    :align: center
    :width: 80%

    Coexistence pin configuration

After finishing with SysConfig settings, be sure to add *IEEE_COEX_ENABLED* inside
*Project Properties* |rarr| *Build* |rarr| *Arm Compiler* |rarr| *Predefined Symbols*
to fully enabled two-wire coexistence operation.

.. figure:: /coexistence/resources/project_ieee-coex-predefine.png
    :align: center
    :width: 80%

    Coexistence predefined symbol