.. _tfm_cc27xx:

Trusted Firmware-M (TF-M)
=========================
The CC27xx implements the Trust Firmware-M (TF-M) version 2.0 for the Secure
Processing Environment (SPE). Additional documentation may be found
`here. <https://www.trustedfirmware.org/projects/tf-m/>`_
The SimpleLink Software Development kit ships with a pre-built TF-M image.
However, rebuilding is supported to allow for customization of the image.

Configuring TF-M
----------------
the |DEVICEHIGH| TF-M configurability options such as Cryptographic algorithm
support and Key Storage parameters may be found in
`<SDK>/tfm_s/cc27xx/production_full/config/config_tfm_project.h`. The
`config_tfm_project.h` header contains documentation and guidance for
configuring the various options.

The memory addresses of the *Secure (S)* and *Non-Secure (NS)* regions can be
modified by editing *<SDK>/tfm_s/cc27xx/production_full/memory_layout.yml*.

If the *NS_ROM_BASE* address is modified, the linker files used to build the NS
application must be modified accordingly to set the correct flash-base address
and size. The linker files (cc27xx*_ns.*) for all compilers are located in
either `<SDK>/source/ti/boards/cc27xxx10` or `<SDK>/source/ti/boards/cc27xxx20`,
depending on the device memory variant. Similarly, if secure boot is enabled,
the Primary Secure and Non-Secure start addresses and length will need to be
updated in SysConfig.

If the "S_ROM_BASE" address is modified, the VTOR must be updated:

- If secure boot is disabled, then the VTOR address can be updated in SysConfig
  under TI DEVICES `-->` Device Configuration `-->` Boot Configuration
  `-->` Application Vector Table. This should be to "S_ROM_BASE" + 0x100 for the
  BL2 header.

- If secure boot is enabled, then the Primary Secure "Start" address should be
  updated to match the "S_ROM_BASE" value. This is controlled via SysConfig
  under TI DEVICES `-->` Device Configuration `-->` Security Configuration `-->`
  Primary Secure. Additionally, "romFixed" in *<SDK Root>/tfm_s/cc27xx/production_full/secure_boot/ti_secure_boot_properties_tfm.json*
  must be set to the value of "S_ROM_BASE" + 0x100.

Building TF-M
-------------
To install the prerequisites tools to build TF-M, go to the
`<SDK>/source/third_party/trusted-firmware-m` folder and run the following:

.. code-block::
    :linenos:

    pip3 install -r tools/requirements.txt


To build the TF-M image, go to the `<SDK>/tfm_s/cc27xx` folder and run the
following:

.. code-block::
    :linenos:

    make clean
    make all

Attestation
-----------
Attestation is the evidence of the device's properties, including the identity
and lifecycle security state of the device. It mitigates impersonation threats
using a cryptographic proof of identity. The combination of an attestation
certificate and token provides both static proof (device identity via
certificate) and dynamic proof (current state via token) of the device’s
trustworthiness. The CC27xx supports attestation according to
`PSA Certified Attestation API 1.0 <https://arm-software.github.io/psa-api/attestation/>`_
with attestation token claims according to `PSA_IOT_PROFILE_1 profile. <https://datatracker.ietf.org/doc/html/draft-tschofenig-rats-psa-token-07>`_

Attestation Token
-----------------
The attestation token is a signed data structure that is generated dynamically
by the device and contains claims about the device's current state. 

This data structure contains:

* Boot Seed

* HW/ROM Version

* Unique HW ID

* Security Lifecycle

* Software Measurements or Configuration Data

* Signature generated using the private key corresponding to the public key in the attestation certificate


For more information, see the `What is an entity attestation token <https://www.psacertified.org/blog/what-is-an-entity-attestation-token/>`_ page.

Token Claims
------------
The following table shows the token claims for PSA_IOT_PROFILE_1 profile.
All mandatory claims are supported.


+--------------------------------+-----------+------------------------------------------------------------------------------------------+------------------------------------------------------------+
| Claim                          | Mandatory | Description                                                                              | Notes                                                      |
+================================+===========+==========================================================================================+============================================================+
| Auth Challenge                 | Yes       | Input object from the caller. For example, this can be a cryptograhpic nonce or a hash   |                                                            |
|                                |           | of locally attested data. The length must be 32, 48, or 64 bytes.                        |                                                            |
+--------------------------------+-----------+------------------------------------------------------------------------------------------+------------------------------------------------------------+
| Instance ID                    | Yes       | Represents the unique identifier of the instance. It is a hash of the public key         |                                                            |
|                                |           | corresponding to the Initial Attestation Key (IAK). If the IAK is a symmetric key then   |                                                            |
|                                |           | the Instance ID is a hash of the IAK. The full definition is in the PSA-SM.              |                                                            |
+--------------------------------+-----------+------------------------------------------------------------------------------------------+------------------------------------------------------------+
| Verification Service Indicator | No        | The value is a text string that can be used to locate the service or a URL specifying    |                                                            |
|                                |           | the address of the service.                                                              |                                                            |
+--------------------------------+-----------+------------------------------------------------------------------------------------------+------------------------------------------------------------+
| Profile Definition             | No        | Contains the name of a document that describes the 'profile' of the report. The document | Value is PSA_IOT_PROFILE_1                                 |
|                                |           | name may include versioning.                                                             |                                                            |
+--------------------------------+-----------+------------------------------------------------------------------------------------------+------------------------------------------------------------+
| Implementation ID              | Yes       | Uniquely identifies the underlying immutable PSA RoT. A verification service can use     | FCFG data will be used to generate the implementation ID:  |
|                                |           | this claim to locate the details of the verification process. Such details include the   |                                                            |
|                                |           | implementation's origin and associated certification state. The full definition is in    | * Die ID (FCFG.deviceInfo.dieid) will be first 16-bytes.   |
|                                |           | the PSA-SM.                                                                              | * MAC BLE (FCFG.deviceInfo.bleAddr) will be next 8-bytes.  |
|                                |           |                                                                                          | * MAC 15.4 (FCFG.deviceInfo.macAddr) will be last 8-bytes. |
+--------------------------------+-----------+------------------------------------------------------------------------------------------+------------------------------------------------------------+
| Client ID                      | Yes       | The Client ID represents the security domain of the caller.                              | Value is -1 when the token is requested by NSPE.           |
|                                |           |                                                                                          |                                                            |
|                                |           | In PSA, a security domain is represented by a signed integer whereby negative values     |                                                            |               
|                                |           | represent callers from the NSPE and where positive IDs represent callers from the SPE.   |                                                            |
|                                |           | The value 0 is not permitted.                                                            |                                                            |
+--------------------------------+-----------+------------------------------------------------------------------------------------------+------------------------------------------------------------+
| Security Lifecycle             | Yes       | Represents the current lifecycle state of the PSA RoT. The state is represented by an    | Lifecycle is dynamically determined based on debug         |
|                                |           | integer that is divided to convey a major state and a minor state. A major state is      | authorization register settings. only the following        |
|                                |           | mandatory and defined by the PSA-SM. A minor state is optional and IMPLEMENTATION        | lifecycle states are attestable:                           |
|                                |           | DEFINED. The PSA security lifecycle state and implementation state are encoded as        |                                                            |
|                                |           | follows:                                                                                 | * PSA_LIFECYCLE_SECURED                                    |
|                                |           |                                                                                          | * PSA_LIFECYCLE_NON_PSA_ROT_DEBUG                          |
|                                |           | * version[15:8]: PSA security lifecycle state.                                           | * PSA_LIFECYCLE_RECOVERABLE_PSA_ROT_DEBUG                  |
|                                |           | * version[7:0]: IMPLEMENTATION DEFINED state.                                            |                                                            |
+--------------------------------+-----------+------------------------------------------------------------------------------------------+------------------------------------------------------------+
| Certification Reference        | No        | Globally unique number in identifying GDSII that went to fabrication, HW and ROM. It can |                                                            |
| (HW Version)                   |           | be used to reference the security level of the PSA-ROT via a certification website.      |                                                            |
|                                |           |                                                                                          |                                                            |
|                                |           | The Certification Reference claim is used to link the class of chip and PSA RoT of the   |                                                            |
|                                |           | attesting device to an associated entry in the PSA Certification database.               |                                                            |
|                                |           |                                                                                          |                                                            |
|                                |           | Format is EAN-13 per the specification.                                                  |                                                            |
+--------------------------------+-----------+------------------------------------------------------------------------------------------+------------------------------------------------------------+
| Boot Seed                      | Yes       | Represents a random value created at system boot time that can allow differentiation of  | When secure boot is enabled, CC27xx boot ROM writes a new  |
|                                |           | of reports from different boot sessions.                                                 | random seed value to Secure RAM at every boot which is     |
|                                |           |                                                                                          | used to populate this claim.                               |
+--------------------------------+-----------+------------------------------------------------------------------------------------------+------------------------------------------------------------+
| Software Components            | Yes       | A list of software components that represent all the software loaded by the PSA Root Of  | This claim is not supported since the CC27xx boot ROM does |
|                                | (see note)| Trust. This claim must be included to be conformant with PSA-SM. Each entry has the      | not support measuring SW components.                       |
|                                |           | following fields:                                                                        |                                                            |
|                                |           |                                                                                          |                                                            |
|                                |           | 1. Measurement type                                                                      |                                                            |
|                                |           | 2. Measurement value                                                                     |                                                            |
|                                |           | 3. Version                                                                               |                                                            |
|                                |           | 4. Signer ID                                                                             |                                                            |
|                                |           | 5. Measurement description                                                               |                                                            |
|                                |           |                                                                                          |                                                            |
|                                |           | This claim is required to be compliant with the PSA-SM.                                  |                                                            |
+--------------------------------+-----------+------------------------------------------------------------------------------------------+------------------------------------------------------------+
| No SW Measurements             | Yes       | In the event that the implementation does not contain any software measurements then the | This claim is included since the SW Components claim is    |
|                                | (see note)| Software Components claim above can be omitted but instead it is mandatory to include    | not supported.                                             |
|                                |           | this claim to indicate this is a deliberate state.                                       |                                                            |
|                                |           |                                                                                          |                                                            |
|                                |           | This claim is intended for devices that are not compliant with the PSA-SM.               |                                                            |
+--------------------------------+-----------+------------------------------------------------------------------------------------------+------------------------------------------------------------+

.. note::
    The *Software Components* claim is mandatory *unless* the *No Software Measurements*
    claim is specified. Otherwise the *No Software Measurements* claim is mandatory.


Security Lifecycle
------------------
The security lifecycle state is determined according to the following activity
diagram whenever the token is requested.

.. figure:: resources/security_lifecycle_diagram.png
    :align: center

    Security Lifecycle Diagram.

Attestation Key
---------------
ECDSA is used to sign the attestation token. The attestation key may be
pre-provisioned by the manufacturer. Upon first device boot, if a
pre-provisioned attestation key (ID = PSA_KEY_ID_IAK) is not found, a random
key pair will be generated and stored in flash for subsequent usage. The public
part of the key pair can be exported by the application for verification of the
token signature.

PSA_KEY_ID_IAK is defined in *<SDK Root>/source/third_party/tfm/interface/include/psa/crypto_values.h*
as follows:

.. code-block:: C

    #define PSA_KEY_ID_IAK ((psa_key_id_t) 0x7fff815d)


Attestation Requirements
------------------------
To ensure the contents of the attestation token can be trusted:

- Secure Boot must be enabled to authenticate the integrity of the TF-M image
  when using attestation since the token claims for boot seed and security
  lifecycle require it.

- Debug authentication in the CCFG must be setup to either FORBID, NON-INVASIVE
  ONLY, or REQUIRE AUTHORIZATION to ensure the correct security lifecycle can
  be reported.  When REQUIRE AUTHORIZATION is selected, only authorized trusted
  users can enter the PSA RoT Debug lifecycle state which allows secure memory
  to be read and potentially written.

Supported APIs
--------------
`PSA Certified Attestation API 1.0 <https://arm-software.github.io/psa-api/attestation/>`_
are supported.

.. code-block:: c
    :linenos:

    /**
     * \brief Get initial attestation token
     *
     * \param[in]     auth_challenge  Pointer to buffer where challenge input is
     *                                stored. Nonce and / or hash of attested data.
     *                                Must be always
     *                                \ref PSA_INITIAL_ATTEST_TOKEN_SIZE bytes
     *                                long.
     * \param[in]     challenge_size  Size of challenge object in bytes.
     * \param[out]    token_buf       Pointer to the buffer where attestation token
     *                                will be stored.
     * \param[in]     token_buf_size  Size of allocated buffer for token, in bytes.
     * \param[out]    token_size      Size of the token that has been returned, in
     *                                bytes.
     *
     * \return Returns error code as specified in \ref psa_status_t
     */
    psa_status_t
    psa_initial_attest_get_token(const uint8_t *auth_challenge,
                                 size_t         challenge_size,
                                 uint8_t       *token_buf,
                                 size_t         token_buf_size,
                                 size_t        *token_size);
    
    /**
     * \brief Get the exact size of initial attestation token in bytes.
     *
     * It just returns with the size of the IAT token. It can be used if the caller
     * dynamically allocates memory for the token buffer.
     *
     * \param[in]   challenge_size  Size of challenge object in bytes. This must be
     *                              a supported challenge size (as above).
     * \param[out]  token_size      Size of the token in bytes, which is created by
     *                              initial attestation service.
     *
     * \return Returns error code as specified in \ref psa_status_t
     */
    psa_status_t
    psa_initial_attest_get_token_size(size_t  challenge_size,
                                      size_t *token_size);


Configurability
---------------
These configurability options are available in *<SDK Root>/tfm_s/cc27xx/production_full/config/config_tfm_project.h*:

.. code-block:: C
    :linenos:

    /* Include optional verification service claim and certification reference
     * claims in initial attestation token.
     *
     * If optional claims are enabled, the certification reference value in
     * <SDK>/source/third_party/tfm/platform/ext/target/ti/cc27xx/attest_hal.c must
     * be updated with the certification number provided by the certification
     * authority.
     */
    #define ATTEST_INCLUDE_OPTIONAL_CLAIMS         0