.. _sec-examples-on-cc2755r10:

Running Software Examples on the CC2755R10
==========================================

.. note::
     The software images built for |DEVICELOW| cannot be directly used on
     |DEVICEHIGH|. The software should be recompiled for |DEVICEHIGH| as described
     below.

Porting Software Examples for CC2755R10
^^^^^^^^^^^^^^^^^^^^^^^^^^^^^^^^^^^^^^^

The CC2755R10 is pin compatible with, and functionally identical to the 
CC2745R10-Q1 device for 2.4 GHz operation. You can run CC2745R10-Q1 software 
examples on the CC2755R10 device without making any changes.

.. note:: The also applies to the CC2745P10-Q1 in relation to CC2755P10 devices

Choosing LaunchPad for Development
^^^^^^^^^^^^^^^^^^^^^^^^^^^^^^^^^^

The |LP_CC27xx| is pin-to-pin compatible with CC2755R10 hardware.  
Therefore the on-board devices of these LaunchPads can be swapped for the 
desired CC2755R10 if specific hardware is not readily available.  The correct 
example project must be selected for the specific device being used.

Moving From LaunchPad to Custom Board
^^^^^^^^^^^^^^^^^^^^^^^^^^^^^^^^^^^^^

You can find instructions on how to design and configure a custom board in the 
:ref:`sec-custom-hardware` chapter.