.. _disable_external_flash_cc23xx:

Disable External Flash
======================

The external flash consumes energy and can be disabled if not used.

By default, SysConfig generates the code to enable / disable the external
flash at the end of ``ti_drivers_config.c``. The functions available to the 
application are: ``Board_sendExtFlashByte``, ``Board_wakeUpExtFlash``, and 
``Board_shutDownExtFlash``.

By default, the ``Board_init`` function disables external flash.