The JSON library provides APIs to parse and build JSON objects.
More...
|
| enum | json_rc_TAG {
JSON_RC__OK = 0,
JSON_RC__RECOVERED__IGNORED_UNKNOWN_VALUE = -1,
JSON_RC__RECOVERED__NESTING_EXCEEDED__IGNORING_LEAVES = -4,
JSON_RC__RECOVERED__PARSING_FAILURE = -5,
JSON_RC__RECOVERED__INVALID_VALUE = -22,
JSON_RC__RECOVERED__NUMBER_ACCURACY_LOSS = -23,
JSON_RC__RECOVERED__NUMBER_OVERFLOW = -24,
JSON_RC__RECOVERED__ILLEGAL_Q_VALUES = -25,
JSON_RC__RECOVERED__STRING_TRUNCATED = -28,
JSON_RC__REWIND_REQUIRED = -99,
JSON_RC__RECOVERABLE_ERROR__MINIMUM_VALUE = -100,
JSON_RC__PARSING_BUFFER_SIZE_EXCEEDED = -101,
JSON_RC__PARSING_FAILURE = -102,
JSON_RC__PARSING_FAILURE__INCOMPLETE_STRING = -103,
JSON_RC__NO_HASH_FOUND = -104,
JSON_RC__BUILDING_UNKNOWN_ATOM = -105,
JSON_RC__BUILDING_BUFFER_SIZE_EXCEEDED = -106,
JSON_RC__BUILDING_PARSED_DATA_EXHAUSTED = -107,
JSON_RC__WRONG_VALUE_SIZE_FOR_TYPE = -108,
JSON_RC__VALUE_NOT_AN_ARRAY = -109,
JSON_RC__INDEX_FAR_BEYOND_ARRAY_END = -110,
JSON_RC__PARSING_BUFFER_SIZE_WOULD_HAVE_EXCEEDED = -111,
JSON_RC__NOT_SUPPORTED = -128,
JSON_RC__NOT_FOUND = -200,
JSON_RC__VALUE_IS_NULL = -201,
JSON_RC__VALUE_NOT_VALID = -202,
JSON_RC__NESTING_EXCEEDED = -204,
JSON_RC__MEMORY_ALLOCATION_ERROR = -300,
JSON_RC__INVALID_TEMPLATE_HANDLE = -301,
JSON_RC__INVALID_OBJECT_HANDLE = -302,
JSON_RC__UNEXPECTED_ERROR = -16384
} |
| |
|
| int16_t | Json_createTemplate (Json_Handle *templateHandle, const char *templateString, uint16_t templateStringLen) |
| | This function creates internal template from the template text. More...
|
| |
| int16_t | Json_destroyTemplate (Json_Handle templateHandle) |
| | This function frees the internal template memory. More...
|
| |
| int16_t | Json_createObject (Json_Handle *objHandle, Json_Handle templateHandle, uint16_t maxObjectSize) |
| | This function creates an empty Json object. More...
|
| |
| int16_t | Json_destroyObject (Json_Handle objHandle) |
| | Free the internal json memory. More...
|
| |
| int16_t | Json_parse (Json_Handle objHandle, char *jsonText, uint16_t jsonTextLen) |
| | This function converts the json text into internal representation. More...
|
| |
| int16_t | Json_getArrayMembersCount (Json_Handle objHandle, const char *pKey) |
| | Retrieve the number of array elements in the provided key. More...
|
| |
| int16_t | Json_getValue (Json_Handle objHandle, const char *pKey, void *pValue, uint16_t *maxValueSize) |
| | This function retrieves value from json. More...
|
| |
| int16_t | Json_setValue (Json_Handle objHandle, const char *pKey, void *pValue, uint16_t valueSize) |
| | Sets the value for the provided key. More...
|
| |
| int16_t | Json_build (Json_Handle objHandle, char *pJsonText, uint16_t *maxTxtLen) |
| | This function builds the internal json into a text json. More...
|
| |
The JSON library provides APIs to parse and build JSON objects.
To access the JSON APIs, the application should include its header file as follows:
And add the following JSON library to the link line:
.../source/ti/utils/json/{toolchain}/{isa}/json_{profile}.a
Usage
This section provides a basic usage summary and a set of examples in the form of commented code fragments. Detailed descriptions of the JSON APIs are provided in subsequent sections.
Synopsis
#define EXAMPLE_JSONBUF \
"{" \
"\"name\": \"John\"," \
"\"age\": 32," \
"\"job\": \"Plumber\"" \
"}"
#define JSON_TEMPLATE \
"{" \
"\"name\": string," \
"\"age\": int32," \
"\"job\": string" \
"}"
Json_parse(objectHandle, EXAMPLE_JSONBUF, strlen(EXAMPLE_JSONBUF));
Examples
The steps of creating a template and allocating memory for a JSON object through Json_createTemplate() and Json_createObject() are required for interacting with JSON objects. The template is what the library uses to know how to parse the JSON it encounters and to format the JSON string it ultimately builds through Json_build().
Creating JSON Objects: The following example demonstrates how to create a JSON object and output it as a string.
#define EXAMPLE_TEMPLATE \
"{" \
"\"name\": string," \
"\"age\": int32," \
"\"job\": string," \
"\"citizen\": boolean" \
"}"
void mainThread() {
bufsize = 256;
char outputBuffer[bufsize];
char *fieldName = "\"age\"";
int32_t ageVal = 42;
bool citizenship = true;
strlen(EXAMPLE_TEMPLATE));
fieldName = "\"citizen\"";
Json_setValue(objectHandle, fieldName, &citizenship,
sizeof(uint16_t));
}
Parsing JSON Objects: The following example demonstrates how to parse a JSON string into memory as a JSON object.
#define EXAMPLE_JSONBUF \
"{" \
"\"name\": \"John\"," \
"\"age\": 32," \
"\"job\": \"Plumber\"," \
"\"citizen\": true" \
"}"
#define EXAMPLE_TEMPLATE \
"{" \
"\"name\": string," \
"\"age\": int32," \
"\"job\": string," \
"\"citizen\": boolean" \
"}"
void mainThread() {
uint16_t bufsize = 32;
char outputBuffer[bufsize];
char *fieldName = "\"job\"";
bool boolBuffer;
uint16_t boolBufSize = sizeof(uint16_t);
strlen(EXAMPLE_TEMPLATE));
Json_parse(objectHandle, EXAMPLE_JSONBUF, strlen(EXAMPLE_JSONBUF));
fieldName = "\"citizen\"";
Json_getValue(objectHandle, fieldName, &boolBuffer, &boolBufSize);
}
Editing JSON Objects: The following example demonstrates parsing a string containing JSON, editing its values, and outputting the updated object.
#define EXAMPLE_TEMPLATE \
"{" \
"\"name\": string," \
"\"age\": int32," \
"\"job\": string" \
"}"
#define EXAMPLE_JSONBUF \
"{" \
"\"name\": \"John\"," \
"\"age\": 32," \
"\"job\": \"Plumber\"" \
"}"
void mainThread() {
uint16_t bufsize = 256;
char outputBuffer[bufsize];
strlen(EXAMPLE_TEMPLATE));
Json_parse(objectHandle, EXAMPLE_JSONBUF, strlen(EXAMPLE_JSONBUF));
Json_setValue(objectHandle,
"\"job\"",
"Contractor", strlen(
"Contractor"));
Json_setValue(objectHandle,
"\"name\"",
"John Sr.", strlen(
"John Sr."));
}
When the JSON objects are no longer needed Json_destroyObject and Json_destroyTemplate should be called:
void snippet() {
strlen(EXAMPLE_TEMPLATE));
...
}
§ JSON_DEFAULT_SIZE
| #define JSON_DEFAULT_SIZE (1024u) |
§ Json_Handle
§ json_rc_T
§ json_rc_TAG
| Enumerator |
|---|
| JSON_RC__OK | |
| JSON_RC__RECOVERED__IGNORED_UNKNOWN_VALUE | |
| JSON_RC__RECOVERED__NESTING_EXCEEDED__IGNORING_LEAVES | |
| JSON_RC__RECOVERED__PARSING_FAILURE | |
| JSON_RC__RECOVERED__INVALID_VALUE | |
| JSON_RC__RECOVERED__NUMBER_ACCURACY_LOSS | |
| JSON_RC__RECOVERED__NUMBER_OVERFLOW | |
| JSON_RC__RECOVERED__ILLEGAL_Q_VALUES | |
| JSON_RC__RECOVERED__STRING_TRUNCATED | |
| JSON_RC__REWIND_REQUIRED | |
| JSON_RC__RECOVERABLE_ERROR__MINIMUM_VALUE | |
| JSON_RC__PARSING_BUFFER_SIZE_EXCEEDED | |
| JSON_RC__PARSING_FAILURE | |
| JSON_RC__PARSING_FAILURE__INCOMPLETE_STRING | |
| JSON_RC__NO_HASH_FOUND | |
| JSON_RC__BUILDING_UNKNOWN_ATOM | |
| JSON_RC__BUILDING_BUFFER_SIZE_EXCEEDED | |
| JSON_RC__BUILDING_PARSED_DATA_EXHAUSTED | |
| JSON_RC__WRONG_VALUE_SIZE_FOR_TYPE | |
| JSON_RC__VALUE_NOT_AN_ARRAY | |
| JSON_RC__INDEX_FAR_BEYOND_ARRAY_END | |
| JSON_RC__PARSING_BUFFER_SIZE_WOULD_HAVE_EXCEEDED | |
| JSON_RC__NOT_SUPPORTED | |
| JSON_RC__NOT_FOUND | |
| JSON_RC__VALUE_IS_NULL | |
| JSON_RC__VALUE_NOT_VALID | |
| JSON_RC__NESTING_EXCEEDED | |
| JSON_RC__MEMORY_ALLOCATION_ERROR | |
| JSON_RC__INVALID_TEMPLATE_HANDLE | |
| JSON_RC__INVALID_OBJECT_HANDLE | |
| JSON_RC__UNEXPECTED_ERROR | |
§ Json_createTemplate()
| int16_t Json_createTemplate |
( |
Json_Handle * |
templateHandle, |
|
|
const char * |
templateString, |
|
|
uint16_t |
templateStringLen |
|
) |
| |
This function creates internal template from the template text.
- Parameters
-
| [out] | templateHandle | template handle |
| [in] | templateString | json template text |
| [in] | templateStringLen | json template text length |
- Returns
- Success: JSON_RC__OK
-
Failure: negative error code
- Example
uint16_t ret;
char *templatestr = "{"
"\"name\":string,"
"\"age\":int32,"
"\"car models\":[string,string,string]}";
strlen(templatestr));
- See also
- Json_destroyTemplate()
§ Json_destroyTemplate()
| int16_t Json_destroyTemplate |
( |
Json_Handle |
templateHandle | ) |
|
This function frees the internal template memory.
- Parameters
-
| [in] | templateHandle | template handle |
- Returns
- Success: JSON_RC__OK
-
Failure: negative error code
- Example
- See also
- Json_createTemplate()
§ Json_createObject()
§ Json_destroyObject()
§ Json_parse()
| int16_t Json_parse |
( |
Json_Handle |
objHandle, |
|
|
char * |
jsonText, |
|
|
uint16_t |
jsonTextLen |
|
) |
| |
This function converts the json text into internal representation.
- Parameters
-
| [in] | objHandle | json object handle |
| [in] | jsonText | pointer to the json text |
| [in] | jsonTextLen | json text size |
- Returns
- Success: JSON_RC__OK
-
Failure: negative error code
- Example
uint16_t ret;
char *jsonBuf = "{\"name\":\"John\","
"\"age\":30,"
"\"car models\":[\"toyota\",\"fiat\",\"volvo\"]}";
- See also
- Json_createObject()
§ Json_getArrayMembersCount()
| int16_t Json_getArrayMembersCount |
( |
Json_Handle |
objHandle, |
|
|
const char * |
pKey |
|
) |
| |
Retrieve the number of array elements in the provided key.
- Parameters
-
| [in] | objHandle | json object handle |
| [in] | pKey | pointer to the key of the requested array |
- Returns
- Success: JSON_RC__OK
-
Failure: negative error code
- Example
uint16_t ret;
uint16_t arrayCount;
char *jsonBuf = "{"
"\"name\":\"John\","
"\"age\":30,"
"\"car models\":[\"toyota\",\"fiat\",\"volvo\"]};
char *key = "\"car models\"";
- See also
- Json_parse()
§ Json_getValue()
| int16_t Json_getValue |
( |
Json_Handle |
objHandle, |
|
|
const char * |
pKey, |
|
|
void * |
pValue, |
|
|
uint16_t * |
maxValueSize |
|
) |
| |
This function retrieves value from json.
- Parameters
-
| [in] | objHandle | json object handle |
| [in] | pKey | pointer to the key of the requested value |
| [out] | pValue | [optional] pointer to the retrieved value |
| [in,out] | maxValueSize | input, number of bytes pValue can hold (if pValue is not NULL). output, number of bytes required to hold requested value. |
- Returns
- Success: JSON_RC__OK
-
Failure: negative error code
- Example
uint16_t ret;
char *jsonBuf = "{"
"\"name\":\"John\","
"\"age\":30,"
"\"car models\":[\"toyota\",\"fiat\",\"volvo\"]};
char *key = "\"name\"";
char value[5];
uint16_t valueSize = 5;
- See also
- Json_parse()
§ Json_setValue()
| int16_t Json_setValue |
( |
Json_Handle |
objHandle, |
|
|
const char * |
pKey, |
|
|
void * |
pValue, |
|
|
uint16_t |
valueSize |
|
) |
| |
Sets the value for the provided key.
- Parameters
-
| [in] | objHandle | json object handle |
| [in] | pKey | pointer to the key of the value to be changed |
| [in] | pValue | pointer to the value to be set |
| [in] | valueSize | size of the value |
- Returns
- Success: JSON_RC__OK
-
Failure: negative error code
- Example
uint16_t ret;
char *jsonBuf = "{"
"\"name\":\"John\","
"\"age\":30,"
"\"car models\":[\"toyota\",\"fiat\",\"volvo\"]};
char *key = "\"age\"";
uint16_r value = 29;
uint16_t valueSize = sizeof(value);
- See also
- Json_parse()
§ Json_build()
| int16_t Json_build |
( |
Json_Handle |
objHandle, |
|
|
char * |
pJsonText, |
|
|
uint16_t * |
maxTxtLen |
|
) |
| |
This function builds the internal json into a text json.
- Parameters
-
| [in] | objHandle | json object handle |
| [out] | pJsonText | pointer to buffer to output the json text |
| [in,out] | maxTxtLen | input, maximum buffer size. output, used buffer size. |
- Returns
- Success: JSON_RC__OK
-
Failure: negative error code
- Example
uint16_t ret;
char *key = "\"age\"";
uint16_r value = 29;
uint16_t valueSize = sizeof(value);
char builtBuff[100];
uint16_t builtBuffSize = 100;
- See also
- Json_parse()
-
Json_setValue()