Logo
Developing with ZBOSS for Zigbee
zb_zgpd_addr_u Union Reference

ZGPD address. More...

#include <zboss_api_zgp.h>

Data Fields

zb_uint32_t src_id
 
zb_ieee_addr_t ieee_addr
 

Detailed Description

ZGPD address.

ZGPD is identified in network whether by SrcId or its IEEE address.

Field Documentation

§ ieee_addr

zb_ieee_addr_t zb_zgpd_addr_u::ieee_addr

ZGPD IEEE address

§ src_id

zb_uint32_t zb_zgpd_addr_u::src_id

ZGPD SrcId

See also
ZGP spec, A.1.4.1.4

The documentation for this union was generated from the following file: