Logo
Developing with ZBOSS for Zigbee
zb_zcl_metering_snapshot_sub_payload_s Union Reference

#include <zb_zcl_metering.h>

Data Fields

zb_zcl_metering_tou_delivered_payload_t tou_delivered
 
zb_zcl_metering_tou_received_payload_t tou_received
 
zb_zcl_metering_block_delivered_payload_t block_delivered
 
zb_zcl_metering_block_received_payload_t block_received
 
zb_zcl_metering_tou_delivered_no_billing_payload_t tou_delivered_no_billing
 
zb_zcl_metering_tou_received_no_billing_payload_t tou_received_no_billing
 
zb_zcl_metering_block_tier_delivered_no_billing_payload_t block_tier_delivered_no_billing
 
zb_zcl_metering_block_tier_received_no_billing_payload_t block_tier_received_no_billing
 

Detailed Description

The format of the Snapshot Sub-Payload differs depending on the SnapshotPayloadType

See also
SE spec, Table D-53 and D.3.2.3.1.7

Field Documentation

§ block_delivered

§ block_received

§ block_tier_delivered_no_billing

§ block_tier_received_no_billing

§ tou_delivered

§ tou_delivered_no_billing

§ tou_received

§ tou_received_no_billing


The documentation for this union was generated from the following file: