Developing with ZBOSS for Zigbee
Data Fields
zb_zcl_attr_var_u Union Reference
Zigbee stack API
»
ZCL API
»
ZCL attributes reporting
Data Fields
zb_uint8_t
u8
zb_int8_t
s8
zb_uint16_t
u16
zb_int16_t
s16
zb_uint24_t
u24
zb_int24_t
s24
zb_uint32_t
u32
zb_int32_t
s32
zb_uint48_t
u48
zb_uint8_t
data_buf
[4]
zb_uint32_t
data_buf_crc32
The documentation for this union was generated from the following file:
/conan-data/ti_zigbee/9.14.00.04/library-lprf/ga/build/f6d18801b7b469a709ae7e8290b03ecdc7a7ad4c/zboss_stable/include/zcl/zb_zcl_reporting.h
Copyright (c) 2012-2022 DSR Corporation, Golden CO, USA.
http://www.dsr-zboss.com
http://www.dsr-corporation.com
ZBOSS documentation. Wed Oct 29 2025.