Parsed Commissioning.ScanResponse structure. More...
#include <zb_zcl_touchlink_commissioning.h>
Data Fields | |
| zb_uint32_t | trans_id |
| Inter-PAN transaction identifier. | |
| zb_uint8_t | rssi_correction |
| RSSI correction. | |
| zb_uint8_t | zb_info |
| Zigbee device information. | |
| zb_uint8_t | zll_info |
| Touchlink information. | |
| zb_uint16_t | key_bitmask |
| Key bitmask. | |
| zb_uint32_t | resp_id |
| Response identifier. | |
| zb_ext_pan_id_t | ext_pan_id |
| Extended Pan ID. | |
| zb_uint8_t | nwk_upd_id |
| Network update identifier. | |
| zb_uint8_t | channel |
| Logical channel. | |
| zb_uint16_t | pan_id |
| Pan ID. | |
| zb_uint16_t | nwk_addr |
| Network address. | |
| zb_uint8_t | n_subdevs |
| Number of sub-devices. | |
| zb_uint8_t | group_ids_total |
| Total group identifiers. | |
| zb_zll_commissioning_ep_info_t | endpoint_info |
| Endpoint information. Shall be present if device has only single endpoint. | |
Parsed Commissioning.ScanResponse structure.