Logo
Developing with ZBOSS for Zigbee
zb_zll_commissioning_network_join_router_res_s Struct Reference

Parsed Commissioning.NetworkJoinRouterResponse payload. More...

#include <zb_zcl_touchlink_commissioning.h>

Data Fields

zb_uint32_t trans_id
 
zb_uint8_t status
 

Detailed Description

Parsed Commissioning.NetworkJoinRouterResponse payload.

See also
ZLL spec, subclause 13.3.2.2.4.

Field Documentation

§ status

zb_uint8_t zb_zll_commissioning_network_join_router_res_s::status

Status.

§ trans_id

zb_uint32_t zb_zll_commissioning_network_join_router_res_s::trans_id

Inter-PAN transaction identifier.


The documentation for this struct was generated from the following file: