Logo
Developing with ZBOSS for Zigbee
zb_zll_commissioning_network_join_end_device_req_s Struct Reference

Parsed Commissioning.NetworkJoinEndDeviceRequest payload. More...

#include <zb_zcl_touchlink_commissioning.h>

Data Fields

zb_uint32_t trans_id
 
zb_ext_pan_id_t ext_pan_id
 
zb_uint8_t key_idx
 
zb_uint8_t encr_nwk_key [16]
 
zb_uint8_t nwk_upd_id
 
zb_uint8_t channel
 
zb_uint16_t pan_id
 
zb_uint16_t short_addr
 
zb_uint16_t group_ids_begin
 
zb_uint16_t group_ids_end
 
zb_uint16_t free_nwk_addrs_begin
 
zb_uint16_t free_nwk_addrs_end
 
zb_uint16_t free_group_ids_begin
 
zb_uint16_t free_group_ids_end
 

Detailed Description

Parsed Commissioning.NetworkJoinEndDeviceRequest payload.

See also
ZCL spec, subclause 13.3.2.1.7.

Field Documentation

§ channel

zb_uint8_t zb_zll_commissioning_network_join_end_device_req_s::channel

Logical channel.

§ encr_nwk_key

zb_uint8_t zb_zll_commissioning_network_join_end_device_req_s::encr_nwk_key[16]

Encrypted network key.

§ ext_pan_id

zb_ext_pan_id_t zb_zll_commissioning_network_join_end_device_req_s::ext_pan_id

Extended Pan ID.

§ free_group_ids_begin

zb_uint16_t zb_zll_commissioning_network_join_end_device_req_s::free_group_ids_begin

Free group identifiers range begin.

§ free_group_ids_end

zb_uint16_t zb_zll_commissioning_network_join_end_device_req_s::free_group_ids_end

Free group identifiers range end.

§ free_nwk_addrs_begin

zb_uint16_t zb_zll_commissioning_network_join_end_device_req_s::free_nwk_addrs_begin

Free network address range begin.

§ free_nwk_addrs_end

zb_uint16_t zb_zll_commissioning_network_join_end_device_req_s::free_nwk_addrs_end

Free network address range end.

§ group_ids_begin

zb_uint16_t zb_zll_commissioning_network_join_end_device_req_s::group_ids_begin

Group identifiers begin.

§ group_ids_end

zb_uint16_t zb_zll_commissioning_network_join_end_device_req_s::group_ids_end

Group identifiers end.

§ key_idx

zb_uint8_t zb_zll_commissioning_network_join_end_device_req_s::key_idx

Key index.

§ nwk_upd_id

zb_uint8_t zb_zll_commissioning_network_join_end_device_req_s::nwk_upd_id

Network update identifier.

§ pan_id

zb_uint16_t zb_zll_commissioning_network_join_end_device_req_s::pan_id

Pan ID.

§ short_addr

zb_uint16_t zb_zll_commissioning_network_join_end_device_req_s::short_addr

Network address.

§ trans_id

zb_uint32_t zb_zll_commissioning_network_join_end_device_req_s::trans_id

Inter-PAN transaction identifier.


The documentation for this struct was generated from the following file: