Logo
Developing with ZBOSS for Zigbee
zb_zll_commissioning_identify_req_s Struct Reference

Parsed Commissioning.IdentifyRequest payload. More...

#include <zb_zcl_touchlink_commissioning.h>

Data Fields

zb_uint32_t trans_id
 Inter-PAN transaction identifier.
 
zb_uint16_t duration
 Identify duration.
 

Detailed Description

Parsed Commissioning.IdentifyRequest payload.

See also
ZCL spec, subclause 13.3.2.1.3.

The documentation for this struct was generated from the following file: