Parsed device information record from the Commissioning.DeviceInformationResponse payload. More...
#include <zb_zcl_touchlink_commissioning.h>
Data Fields | |
| zb_ieee_addr_t | ieee_addr |
| zb_uint8_t | ep_id |
| zb_uint16_t | profile_id |
| zb_uint16_t | device_id |
| zb_uint8_t | version |
| zb_uint8_t | group_id_count |
| zb_uint8_t | sort |
Parsed device information record from the Commissioning.DeviceInformationResponse payload.
| zb_uint16_t zb_zll_commissioning_device_information_ep_info_res_s::device_id |
Device identifier.
| zb_uint8_t zb_zll_commissioning_device_information_ep_info_res_s::ep_id |
Device's endpoint identifier.
| zb_uint8_t zb_zll_commissioning_device_information_ep_info_res_s::group_id_count |
Group identifier count.
| zb_ieee_addr_t zb_zll_commissioning_device_information_ep_info_res_s::ieee_addr |
IEEE address of the sub-device.
| zb_uint16_t zb_zll_commissioning_device_information_ep_info_res_s::profile_id |
Profile identifier.
| zb_uint8_t zb_zll_commissioning_device_information_ep_info_res_s::sort |
Sort.
| zb_uint8_t zb_zll_commissioning_device_information_ep_info_res_s::version |
Device version.