Logo
Developing with ZBOSS for Zigbee
zb_zgps_mapping_entry_generic_switch_option_data_s Struct Reference

Mapping table entry additional info generic switch option data structure Figure 85 – Format of the Option data of the Generic switch command execution option of the Translation Table entry. More...

#include <zboss_api_zgp.h>

Data Fields

zb_uint8_t contact_status
 
zb_uint8_t contact_bitmask
 

Detailed Description

Mapping table entry additional info generic switch option data structure Figure 85 – Format of the Option data of the Generic switch command execution option of the Translation Table entry.


The documentation for this struct was generated from the following file: