Logo
Developing with ZBOSS for Zigbee
zb_zdo_system_server_discovery_req_s Struct Reference

Request parameters for System_Server_Discovery_req. More...

#include <zboss_api_zdo.h>

Data Fields

zb_uint16_t server_mask
 

Detailed Description

Request parameters for System_Server_Discovery_req.

See also
ZB spec, subclause 2.4.3.1.13.

Field Documentation

§ server_mask

zb_uint16_t zb_zdo_system_server_discovery_req_s::server_mask

Server mask for device discovery


The documentation for this struct was generated from the following file: