Header of simple_desc_resp primitive. More...
#include <zboss_api_zdo.h>
Data Fields | |
| zb_uint8_t | tsn |
| zb_uint8_t | status |
| zb_uint16_t | nwk_addr |
| zb_uint8_t | length |
Header of simple_desc_resp primitive.
| zb_uint8_t zb_zdo_simple_desc_resp_hdr_s::length |
Length of the simple descriptor
| zb_uint16_t zb_zdo_simple_desc_resp_hdr_s::nwk_addr |
NWK address for the request
| zb_uint8_t zb_zdo_simple_desc_resp_hdr_s::status |
The status of the Desc_req command. zdp_status
| zb_uint8_t zb_zdo_simple_desc_resp_hdr_s::tsn |
ZDP transaction sequence number