Parameters of Simple_desc_req primitive. More...
#include <zboss_api_zdo.h>
Data Fields | |
| zb_uint16_t | nwk_addr |
| zb_uint8_t | endpoint |
Parameters of Simple_desc_req primitive.
To be put into buffer as data (means - after space alloc).
| zb_uint8_t zb_zdo_simple_desc_req_s::endpoint |
The endpoint on the destination
| zb_uint16_t zb_zdo_simple_desc_req_s::nwk_addr |
NWK address that is used for IEEE address mapping.