Parameters of zb_zdo_raw_resp call. More...
#include <zboss_api_zdo.h>
Data Fields | |
| zb_uint16_t | cluster_id |
| zb_uint16_t | src_addr |
Parameters of zb_zdo_raw_resp call.
| zb_uint16_t zb_zdo_raw_resp_param_s::cluster_id |
The identifier of the object in the response.
| zb_uint16_t zb_zdo_raw_resp_param_s::src_addr |
Source address of a device that sent a response