NWK_addr_req response frame. More...
#include <zboss_api_zdo.h>
Data Fields | |
| zb_uint8_t | tsn |
| zb_uint8_t | status |
| zb_ieee_addr_t | ieee_addr |
| zb_uint16_t | nwk_addr |
NWK_addr_req response frame.
| zb_ieee_addr_t zb_zdo_nwk_addr_resp_head_s::ieee_addr |
64-bit address for the Remote Device.
| zb_uint16_t zb_zdo_nwk_addr_resp_head_s::nwk_addr |
16-bit address for the Remote Device.
| zb_uint8_t zb_zdo_nwk_addr_resp_head_s::status |
The status of the NWK_addr_req command.
| zb_uint8_t zb_zdo_nwk_addr_resp_head_s::tsn |
ZDP transaction sequence number