Parameters for Mgmt_Permit_Joining_req. More...
#include <zboss_api_zdo.h>
Data Fields | |
| zb_uint8_t | permit_duration |
| zb_uint8_t | tc_significance |
Parameters for Mgmt_Permit_Joining_req.
| zb_uint8_t zb_zdo_mgmt_permit_joining_req_s::permit_duration |
The length of time in seconds. 0x00 and 0xff indicate that permission is disabled or enabled
| zb_uint8_t zb_zdo_mgmt_permit_joining_req_s::tc_significance |
If this is set to 0x01 and the remote device is the Trust Center, the command affects the Trust Center authentication policy as described in the sub-clauses below; According to r21, should be always set to 0x01.