Logo
Developing with ZBOSS for Zigbee
zb_zdo_mgmt_nwk_ieee_joining_list_rsp_s Struct Reference

Response for Mgmt_NWK_IEEE_Joining_List_rsp. More...

#include <zboss_api_zdo.h>

Data Fields

zb_uint8_t tsn
 
zb_uint8_t status
 
zb_uint8_t ieee_joining_list_update_id
 
zb_uint8_t joining_policy
 
zb_uint8_t ieee_joining_list_total
 
zb_uint8_t start_index
 
zb_uint8_t ieee_joining_count
 

Detailed Description

Response for Mgmt_NWK_IEEE_Joining_List_rsp.

See also
ZB spec, subclause 2.4.4.4.11.

Field Documentation

§ status

zb_uint8_t zb_zdo_mgmt_nwk_ieee_joining_list_rsp_s::status

The status of the Mgmt_NWK_IEEE_Joining_List_req command.

§ tsn

zb_uint8_t zb_zdo_mgmt_nwk_ieee_joining_list_rsp_s::tsn

ZDP transaction sequence number


The documentation for this struct was generated from the following file: