Logo
Developing with ZBOSS for Zigbee
zb_zdo_mgmt_lqi_param_s Struct Reference

Parameters for Mgmt_Lqi_req. More...

#include <zboss_api_zdo.h>

Data Fields

zb_uint8_t start_index
 
zb_uint16_t dst_addr
 

Detailed Description

Parameters for Mgmt_Lqi_req.

See also
ZB spec, subclause 2.4.3.3.2.

Field Documentation

§ dst_addr

zb_uint16_t zb_zdo_mgmt_lqi_param_s::dst_addr

destination address

§ start_index

zb_uint8_t zb_zdo_mgmt_lqi_param_s::start_index

Starting Index for the requested elements of the Neighbor Table


The documentation for this struct was generated from the following file: