#include <zboss_api_zdo.h>
Data Fields | |
| zb_uint8_t | tsn |
| zb_uint8_t | status |
| zb_ieee_addr_t | ieee_addr_remote_dev |
| zb_uint16_t | nwk_addr_remote_dev |
brief ZDO IEEE address response frame
| zb_ieee_addr_t zb_zdo_ieee_addr_resp_s::ieee_addr_remote_dev |
64-bit address for the Remote Device.
| zb_uint16_t zb_zdo_ieee_addr_resp_s::nwk_addr_remote_dev |
16-bit address for the Remote Device.
| zb_uint8_t zb_zdo_ieee_addr_resp_s::status |
The status of the NWK_addr_req command.
| zb_uint8_t zb_zdo_ieee_addr_resp_s::tsn |
ZDP transaction sequence number