Active EP response. More...
#include <zboss_api_zdo.h>
Data Fields | |
| zb_uint8_t | tsn |
| zb_uint8_t | status |
| zb_uint16_t | nwk_addr |
| zb_uint8_t | ep_count |
Active EP response.
| zb_uint8_t zb_zdo_ep_resp_s::ep_count |
The count of active endpoints on the Remote Device.
| zb_uint16_t zb_zdo_ep_resp_s::nwk_addr |
NWK address for the request.
| zb_uint8_t zb_zdo_ep_resp_s::status |
The status of the Active_EP_req command.
| zb_uint8_t zb_zdo_ep_resp_s::tsn |
ZDP transaction sequence number