Logo
Developing with ZBOSS for Zigbee
zb_zdo_end_device_bind_req_tail_s Struct Reference

End_Device_Bind_req command head. More...

#include <zboss_api_zdo.h>

Data Fields

zb_uint8_t num_out_cluster
 

Detailed Description

End_Device_Bind_req command head.

See also
ZB spec, subclause 2.4.3.2.1.

Field Documentation

§ num_out_cluster

zb_uint8_t zb_zdo_end_device_bind_req_tail_s::num_out_cluster

The number of Output Clusters provided for matching within OutClusterList


The documentation for this struct was generated from the following file: